Part Number: LAUNCHXL-CC1352P
Other Parts Discussed in Thread: ENERGYTRACE
Tool/software: Code Composer Studio
Energytrace seems to report the wrong current. I need to power cycle the board, or re-start energy trace a few times to get the expected current.
Steps:
1.Load hex file to board
2.start energy trace via icon near the menu
3.press the green triangle button (play button)
4.Look at mean current, reads ~0.654mA (should be ~50uA)
5.Re-start and/or power cycle launchpad
6.press the green triangle button (play button)
7.Look at mean current, reads ~0.654mA or reads 0.050mA. If it reads the former repeat process
Also sometime energytrace hangs for unknown reasons
My Setup
Ubuntu18
CCS v9.3
SDK v3.40
Any thoughts?