Other Parts Discussed in Thread: TMDSLCDK138, OMAPL138
Tool/software: TI C/C++ Compiler
I am n the process of ordering the TMDSLCDK138 EVM board, but read in the literature that the board doeasnt come with the XDS JTAG board for debugging. Is this a must to have a real time DSP code on the target? . Also, I have located the XDS110 JTAG Debug Probe in case I must have it.
I am also wondering which user interface board I need to use (if any), I noticed from older you tube videos , a user interface board is mounted on the board(this dates back to 2011 though). Not sure what choices I have here regarding a user interface board (the board used on that video is zoom opm138?) .
My last question is I run my software on Mac OS . I have installed already Code Composer Studio and runs fine on it (Mac OS Sierra v10.13.6),
I noticed from reading the literature that to run the various debuggers and software of the real time DSP , the platforms that are supported are windows and linux. So, is the TI RTOS is compatible with MAC OSX? or do I have to install a virtual linux environment in parallel? . Thank you