This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Bit manipulation for 16 bits register

I am coding a sample code for MSP430G2xx on CCS4.

In  this sample project , I want to configure the register by bit access.

In my head file ,  I build a bit access union for each register like below.

When I using it to configure the bit field as this "TACTL.bits.TASSELx = 3 ;", 

in fact, "TAIFG" and "TAIE " bit field  was changed.   -  -|||

But,  "TACTL.bits.MCx  = 2;   TACTL.bits.IDx  = 2" works well.

Has anybody try "Bit manipulation for 16 bits register" in CCS for MSP430 ?

 

/******************** source code start ***********************/

 

union TACTL_16BITS

{    

    unsigned int u2Reg;

    struct

    {

    unsigned int TAIFG : 1;

    unsigned int TAIE : 1;

    unsigned int TACLR : 1;

    unsigned int _LBIT3 : 1;

    unsigned int MCx   : 2;

    unsigned int IDx   : 2;

    unsigned int TASSELx : 2;

    unsigned int _BITx : 6;

    }bits;

};

extern volatile union TACTL_16BITS TACTL;

/********************** source code end ******************************/