This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/MSP430F5418A: Error: output file "XXXXXX.out" exceeds code size limit

Part Number: MSP430F5418A

Tool/software: Code Composer Studio

Hello

I am facing error in CCS6.2  that . out file can not generated as the code size exceeds  size limit. 

The compiler used is TI v15.12.3.LTS

I am using MSP430F5418A controller which is having 128KB program memory. I am developing code for one of our product. At some point even I try to add a single line of code the compiler is unable to compiler it successfully.  Before it the code compiles successfully.  I can see the memory allocation in CCS, it shows I have enough memory available to add Code. Please refer the below photo. I want to add more functions in my code but unable to do it as the compiler gives the error.

Please suggest me how to overcome such issues. Is it related with compiler version?