This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/LAUNCHXL-CC1312R1: IRDA CC1312R1

Part Number: LAUNCHXL-CC1312R1
Other Parts Discussed in Thread: TIDA-01212

Tool/software: Code Composer Studio

Dear Sir/madam,

I am migrating my water meter project STM32 to CC1312R2.

One of its feature is the IRDA, we used STM library(UART) so the IRDA can be done easily.

But for the CC1312R2, we only find the TIDA-01212 of the SCS version which we still need to put a lof ot effort in coding and testing,

We wanna ask any Demo or example of IRDA was done and test on CC1312R2 without external IC , so we can put minimmal effort on hardware and coding effect.

Thanks

Jeff

  • Hi,

    You can find a SLA lab here dealing with IR generation.

    FYI (and expecting this will save you some time), I went quickly into the code and I mentioned a small mistake. In IRGENCC26XX.c there are several Power Driver calls with PowerCC26XX_IDLE_PD_DISALLOW. According to PowerCC26XX.h this define is deprecated. They should be replaced with PowerCC26XX_DISALLOW_IDLE . 

    If you need further assistance in the porting effort, please don't hesitate to contact your local sales team.

    Best regards,

  • Hi Jeff,

    There is a "IR generation Simplelink Acadamy lab available for CC2640R2 that could maybe be helpful but beside from this, there is no examples other than the  TIDA design and that code as far as I'm aware.

    dev.ti.com/.../node