This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/PROCESSOR-SDK-DRA8X-TDA4X: XDS 110 USB Debug Probe Error -1060

Part Number: PROCESSOR-SDK-DRA8X-TDA4X

Tool/software: Code Composer Studio

Hello,

I'm facing the following error when I try the procedure described in psdk_rtos_auto_j7_06_01_01_12/psdk_rtos_auto/docs/user_guide/ccs_setup_j721e.html#using-ccs-debug-with-linux-on-a72:

"C66xx_0: Error connecting to the target: (Error -1060 @ 0x0) Device is not responding to the request. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 8.4.0.00006)"

I managed to make it work a few days ago, but now I cannot connect to the C66 core 0 any longer. I tried to reboot the J721EX EVM board, create a new workspace and recreate the target configuration file, without success. Strangely, I also tried to connect to the C66 core 1, Cortex-R5 and Cortex-A72 and they work properly.

Thanks for your help,

Fernando A. Endo