This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS / IWR1843: HOW TO SET 3tx bpm mode

Part Number: IWR1843

Tool/software: Code Composer Studio

I have to use  IWR1843 without DCA1000. Now I want to set 3tx bpm mode,but I do not know the steps.

Thank you if you can help me.

  • Hi, there:

    If you check SDK users guide and search for bpmCfg, you can find the information below:

    Every frame should consist of alternating chirps with pattern TXA+TxB and TXA-TXB where TXA and TXB are two azimuth TX antennas. This is alternate configuration to TDM-MIMO scheme and provides SNR improvement by running 2Tx simultaneously. When using this scheme, user
    should enable both the azimuth TX in the chirpCfg. See profile_2d_bpm.cfg profile in the xwr16xx mmW demo profiles directory for example usage.
    This config is supported and mandatory only for demos that use Doppler DSP DPU (xwr16xx/xwr68xx). This config is not supported and is not needed for demos that use Doppler HWA DPU (xwr18xx/xwr64xx).

    So, we only support 2TX BPM.   For 3 TX BPM, we do not have a system solution yet.  But if you need help to configure on the chirp configuration level, we probably can help.  Can you explain what functionality you need to enable 3 TX BPM mode?

    Best,

    Zigang

  • HI,

    Hope your problem has resolved.  Since I am not hearing from you for a long time, I am closing this thread. 

    Best,

    Zigang