Part Number: TDA4VM
Tool/software: TI C/C++ Compiler
I am using C7000 CGT for windows to simulate C7X. The version is 1.3.0.My visual studio version is 2019.
I executed this code.
Vout.lo = __SE1ADV(uint4);
But it only loaded one element.
Henry
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TDA4VM
Tool/software: TI C/C++ Compiler
Henry,
I'm not sure what your problem could be. Can you try to compile and run the following code in your environment? Also, it would be helpful if you posted/attached your code.
#include <c7x.h>
#include <stddef.h>
#include <stdio.h>
#define SIZE_ARRAY (1024)
uint uint_array[SIZE_ARRAY];
void init_memory()
{
for (int i = 0; i < SIZE_ARRAY; i++)
uint_array[i] = i + 1;
}
uint8 se_func(uint32_t *startaddr)
{
uint8 Vresult;
__SE_TEMPLATE_v1 params = __gen_SE_TEMPLATE_v1(); // SE PARAMETERS
params.DIMFMT = __SE_DIMFMT_2D;
params.ELETYPE = __SE_ELETYPE_32BIT;
params.VECLEN = __SE_VECLEN_4ELEMS; // 4 ELEMENTS
// SETUP TEMPLATE VECTOR BASED ON SETTINGS AND OPEN THE STREAM
// BASED ON ITERATION COUNTERS AND DIMENSIONS (IN TERMS OF # OF ELEMS)
params.ICNT0 = 128;
params.ICNT1 = 128;
params.DIM1 = 0;
params.ICNT2 = 128;
params.DIM2 = 0;
params.ICNT3 = 128;
params.DIM3 = 0;
// DECDIM1 WIDTH (0 by default)
params.DECDIM1_WIDTH = 0;
// DECDIM2 WIDTH (0 by default)
params.DECDIM2_WIDTH = 0;
// LEZR COUNT (0 by default)
params.LEZR_CNT = 0;
__SE1_OPEN((void*)startaddr, params);
// READ THE STREAM AND ADVANCE THE COUNTERS
for (int I0 = 0; I0 < 8; I0++)
{
printf("-----------------\n");
uint8 Vout =
#ifdef __C7X_HOSTEM__
uint8(0);
#else
(uint8)(0);
#endif
Vout.lo = __SE1ADV(uint4);
#ifdef __C7X_HOSTEM__
Vout.print();
#else
printf("%d,%d,%d,%d,%d,%d,%d,%d\n", Vout.s0, Vout.s1, Vout.s2, Vout.s3, Vout.s4, Vout.s5, Vout.s6, Vout.s7);
#endif
Vout.hi = __SE1ADV(uint4);
#ifdef __C7X_HOSTEM__
Vout.print();
#else
printf("%d,%d,%d,%d,%d,%d,%d,%d\n", Vout.s0, Vout.s1, Vout.s2, Vout.s3, Vout.s4, Vout.s5, Vout.s6, Vout.s7);
#endif
Vresult += Vout;
}
// CLOSE THE STREAM
__SE1_CLOSE();
return Vresult;
}
int main()
{
init_memory();
se_func(uint_array); // Not using the return value
return 0;
}
Hi,
Thank you for the reply.This is the code I executed.
#include <c7x.h>
#include <stddef.h>
uint8 se_func(uint32_t *startaddr)
{
int I0;
uint8 Vresult;
__SE_TEMPLATE_v1 params = __gen_SE_TEMPLATE_v1(); // SE PARAMETERS
params.DIMFMT = __SE_DIMFMT_4D;
params.ELETYPE = __SE_ELETYPE_32BIT;
params.VECLEN = __SE_VECLEN_4ELEMS; // 4 ELEMENTS
// SETUP TEMPLATE VECTOR BASED ON SETTINGS AND OPEN THE STREAM
// BASED ON ITERATION COUNTERS AND DIMENSIONS (IN TERMS OF # OF ELEMS)
params.ICNT0 = 4;
params.ICNT1 = 2;
params.DIM1 = 4;
params.ICNT2 = 2;
params.DIM2 = 8;
params.ICNT3 = 4;
params.DIM3 = -16;
// DECDIM1 WIDTH (0 by default)
params.DECDIM1_WIDTH = 0;
// DECDIM2 WIDTH (0 by default)
params.DECDIM2_WIDTH = 0;
// LEZR COUNT (0 by default)
params.LEZR_CNT = 0;
__SE1_OPEN((void*)startaddr, params);
// READ THE STREAM AND ADVANCE THE COUNTERS
for (I0 = 0; I0 < 8; I0++)
{
uint8 Vout;
Vout.lo = __SE1ADV(uint4);
Vout.hi = __SE1ADV(uint4);
Vresult += Vout;
}
// CLOSE THE STREAM
__SE1_CLOSE();
return Vresult;
}
And I executed your code, this is the print information.
Henry,
I'm going to look into this issue with host emulation and the MS Visual Studio compiler. In the meantime, could you try the g++ compiler and let me know what happens?
Just for reference, the expected output for the code I posted above is (and the output I get with g++):
-----------------
(1, 2, 3, 4, 0, 0, 0, 0)
(1, 2, 3, 4, 5, 6, 7, 8)
-----------------
(9, 10, 11, 12, 0, 0, 0, 0)
(9, 10, 11, 12, 13, 14, 15, 16)
-----------------
(17, 18, 19, 20, 0, 0, 0, 0)
(17, 18, 19, 20, 21, 22, 23, 24)
-----------------
(25, 26, 27, 28, 0, 0, 0, 0)
(25, 26, 27, 28, 29, 30, 31, 32)
-----------------
(33, 34, 35, 36, 0, 0, 0, 0)
(33, 34, 35, 36, 37, 38, 39, 40)
-----------------
(41, 42, 43, 44, 0, 0, 0, 0)
(41, 42, 43, 44, 45, 46, 47, 48)
-----------------
(49, 50, 51, 52, 0, 0, 0, 0)
(49, 50, 51, 52, 53, 54, 55, 56)
-----------------
(57, 58, 59, 60, 0, 0, 0, 0)
(57, 58, 59, 60, 61, 62, 63, 64)
Henry,
It appears MS Visual C++ cannot pack bitfields like gcc/g++ can. Furthermore, the implementation of the SE setup register and SA setup register is dependent upon this bitfield packing behavior. It seems the previous C7000 compiler package worked in some cases with MS Visual C++ because there were _set* functions that did the bitfield packing of the SE setup register manually. Although we were all probably all still getting lucky there as some bitfields in the SE setup register didn't have a "set" function to do the bitpacking. (The v1.3 C7000 compiler changed the API to the SE and SA setup registers to make it cleaner and more extensible. Thus, those "set" functions were removed from the API.)
In short, it appears MS Visual C++ cannot be used for Host Emulation (at least at this time). g++ must be used instead.
I will add a work-item to the team that involves fixing the issue (not sure if this can be done) or documenting that MS Visual C++ won't work with host emulation.
-Todd