Part Number: MSP430FR5989-EP
Tool/software: Code Composer Studio
I have two MSP430 evaluation boards connected to my Windows system (each through a different USB switch, else Windows will only see one, but that's a different issue!).
The two boards talk to each other over SPI, so I need them both online and working.
If I flash or debug my software, CCS picks the USB debug port with the lowest number.
Is there a way to somewhere specify which USB debug port CCS should use?
I checked the debug configuration: under Target there is a 'Device' drop down box, but it's grayed out.
Any ideas?