Part Number: AWR1843
Tool/software: Code Composer Studio
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: AWR1843
Tool/software: Code Composer Studio
Your device has both ARM and C6000 CPU cores on it. I'll answer for both compilers. For the TI ARM compiler #include <arm_acle.h>. For the C6000 compiler, #include <c6x.h>. That will provide a function prototype for most of the intrinsics. That said, these include files are not tested to solve your particular problem, so you might encounter some gaps.
Thanks and regards,
-George
Thanks for your reply.
We had a look at those files but we didn't find some intrinsics prototype, e.g. _amemd8.
Is it possible that some other .h files are generated at compile time and so they're not really accessible before?
Thanks again for your support,
Matteo
Unfortunately, those header files are the best solution we have for your particular problem.
Matteo Sticco said:Is it possible that some other .h files are generated at compile time and so they're not really accessible before?
Unfortunately, no.
Thanks and regards,
-George
Hello,
I think I resolved the issue.
I created an header file containing the prototypes of the intrinsics I needed and I used a #define in order to prevent the compiler to see them. At the same time this #define is added to the configuration file of flexelint to let it recognize them.
Hope this will help anyone who has the same problem!
Regards,
Matte Sticco