I'm new to TI processors and have a question regarding flash programming of the F28xx devices with a Blackhawk XDS100v2(D).
I currently am trying to understand if it is possible (and if so, how) to program F28xx and Delfino processors.
Can I do it with a stand alone flash burner app, and/or can I do it with CCS 3.3 and/or CCS 4.x?
If not, do I need to change programmers and upgrade CCS4?
We are using CCS 3.3 and CCS 4.0 but only have the free version of CCS 4.0 that comes
with the XDS100v2. If so where can I get information on the tools required to flash the devices with XDS100v2.
Some web sites I have seen listed that it is possible, but looking at others it doesn't seem so. The reason I purchased the XDS100v2 is because it gave
me the full CCS 4 for the C2000 devices, however if it can't flash the parts, it doesn't seem very useful. I just need to be able to load compiled *.out files to the parts.
Thanks for your help.