Part Number: TMS320F28335
Tool/software: Code Composer Studio
Hi Dear E2E Support
I am using the DSP Development Board with the TMS320F28335 control card and the communication with PC is done using TID60000467 cable (USB/RS232 cable). Also, I am using PSIM V12.02 and I try to run one of their examples that done on the tutorial video and I follow all the steps carefully and I make sure everything seems working fine with only two warning on the problems window shows as follow:
1.Description Resource Path Location Type
#10063-D entry-point symbol other than "_c_int00" specified: "code_start" 3_ph_sine_wave_with_SCI_monitoring C/C++ Problem
2. Description Resource Path Location Type
Invalid project path: Include path not found (\packages\ti\xdais). 3_ph_sine_wave_with_SCI_monitoring path entry Problem
Note: the name of the generated code from PSIM is 3_ph_sine_wave_with_SCI_monotoring.
However, the program is running and I test the communication and it give me success. Thus, I go back to PSIM to run the DSP oscilloscope and i connect it with the DSP successfully but it does not show any input or output values at all. Please any ideas or help. I am very new using the DSP board.
Also a picture from PSIM for the DSP oscilloscope