Part Number: MSP430FR5994
Tool/software: TI C/C++ Compiler
Hello,
I have a piece of code written using code composer studio which I need to convert to work with GNUC. This code uses SPI and has an SPI interrupt.
I am struggling regarding how to use the reading and writing higher FRAM in GNUC.
In code composer studio, I have used two functions __data20_write_char and __data20_read_char. I am not sure how to do this in when I compile with GCC.
In this code
#include <stdio.h>
#include "spi.h"
uint8_t *ReceiveBuffer;
int16_t RXByteCtr;
int16_t ReceiveIndex;
uint8_t *TransmitBuffer;
int16_t TXByteCtr;
int16_t TransmitIndex;
uint8_t is_send_fram;
uint8_t is_recv_fram;
static void SendUCB1Data(uint8_t val)
{
while (!(UCB1IFG & UCTXIFG))
; // USCI_B1 TX buffer ready?
UCB1TXBUF = val;
}
void initSPI()
{
SLAVE_CS_DIR |= SLAVE_CS_PIN; //Here CS PIn is 5.3
SLAVE_CS_OUT |= SLAVE_CS_PIN;
// Configure SPI
P5SEL0 |= BIT0 | BIT1 | BIT2;
//Clock Polarity: The inactive state is high
//MSB First, 8-bit, Master, 3-pin mode, Synchronous
UCB1CTLW0 = UCSWRST; // **Put state machine in reset**
UCB1CTLW0 |= UCCKPL | UCMSB | UCSYNC
| UCMST | UCSSEL__SMCLK; // 3-pin, 8-bit SPI Slave
UCB1BRW = 0x08;
//UCB1MCTLW = 0;
UCB1CTLW0 &= ~UCSWRST; // **Initialize USCI state machine**
UCB1IE |= UCRXIE; // Enable USCI0 RX interrupt
}
void spi_transfer(uint8_t *send, uint8_t *recv, uint16_t send_len,
uint16_t recv_len, uint8_t send_fram, uint8_t recv_fram)
{
TXByteCtr = send_len - 1;
RXByteCtr = recv_len;
ReceiveIndex = -1;
TransmitIndex = 1;
TransmitBuffer = send;
ReceiveBuffer = recv;
is_send_fram = send_fram;
is_recv_fram = recv_fram;
SLAVE_CS_OUT &= ~(SLAVE_CS_PIN);
SendUCB1Data(send[0]);
__bis_SR_register(CPUOFF + GIE); // Enter LPM0 w/ interrupts
SLAVE_CS_OUT |= SLAVE_CS_PIN;
}
//******************************************************************************
// SPI Interrupt ***************************************************************
//******************************************************************************
#if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__)
#pragma vector=USCI_B1_VECTOR
__interrupt void USCI_B1_ISR(void)
#elif defined(__GNUC__)
void __attribute__ ((interrupt(USCI_B1_VECTOR))) USCI_B1_ISR (void)
#else
#error Compiler not supported!
#endif
{
uint8_t ucb1_rx_val = 0;
uint8_t data;
switch (__even_in_range(UCB1IV, USCI_SPI_UCTXIFG))
{
case USCI_NONE:
break;
case USCI_SPI_UCRXIFG:
ucb1_rx_val = UCB1RXBUF;
UCB1IFG &= ~UCRXIFG;
if (TXByteCtr)
{
if (is_send_fram) {
data = __data20_read_char((unsigned long int)&TransmitBuffer[TransmitIndex++]);
} else {
data = TransmitBuffer[TransmitIndex++];
}
SendUCB1Data(data);
TXByteCtr--;
}
else if (RXByteCtr)
{
if (ReceiveIndex == -1)
{
ReceiveIndex = 0;
SendUCB1Data(DUMMY);
}
else
{
if (is_recv_fram) {
__data20_write_char((unsigned long int)&ReceiveBuffer[ReceiveIndex++], ucb1_rx_val);
} else {
ReceiveBuffer[ReceiveIndex++] = ucb1_rx_val;
}
if (--RXByteCtr > 0)
{
SendUCB1Data(DUMMY);
}
else
{
__bic_SR_register_on_exit(CPUOFF);
}
}
}
else
{
__bic_SR_register_on_exit(CPUOFF); // Exit LPM0
}
//__delay_cycles(1000);
break;
case USCI_SPI_UCTXIFG:
break;
default:
break;
}
}