Part Number: TMS320C5505
Tool/software: Code Composer Studio
Hi,
My customer is trying to migrate from CCSv5.5 to CCSv6.2. The host PC is windows 10.
The steps they tried were below;
1) Uninstall CCSv5.5 from PC
2) Install CCSv6.2
3) Install DSP/BIOS_5.42.01.09
4) Open CCSv6.2 with v5.5 workspace. Below dialogue box appears.
--------------------------------------------------------------------------------
Workspace 'C:/work/[name of workspace]' was written with an older version of the product and will be updated.
Updating the workspace can make it incompatible with older versions of the product.
Are you sure want to continue with this workspace?
[OK] [Cancel]
--------------------------------------------------------------------------------
5) Select [OK]
6) Import project from the updated workspace.
7) Rebuild the project gives below error.
**** Build of configuration Debug for project dsp_app ****
"C:\\ti\\ccsv6\\utils\\bin\\gmake" all
'Building file: ../[name of project].tcf'
'Invoking: TConf'
"C:/ti/bios_5_42_01_09/xdctools/tconf" -b -Dconfig.importPath="C:/ti/bios_5_42_01_09/packages;" "../[name of project].tcf"
subdir_rules.mk:14: recipe for target 'build-1984884193' failed
C:\ti\bios_5_42_01_09\xdctools\C:/ti/bios_5_42_01_09/xdctools/tconf: can't create session manager: create of JVM failed
gmake: *** [build-1984884193] Error 1
**** Build Finished ****
Could you help me how to solve the issue?
Thanks and regards,
Koichiro Tashiro