This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/LDC1614: LDC1614

Part Number: LDC1614

Tool/software: Code Composer Studio

Hi,

i am using LDC1614 with TivaC123, i can read a gap up to 20 mm using the internal coil fixed in the sensor board, but when using the same coil as an external one the resolution decreased with a large value, as while increasing the gap the change in inductance decreases.

can any one tell me what is the problem with this, and what is you recommend me to do !!