Tool/software: Code Composer Studio
Hi sir,
I want to test CAN-FD in IWR6843ISK ES2.0.
For that, I'm load the "xwr68xx_canfd_mss.xer4f" which in the canfd test folder.
PATH : "C:\ti\mmwave_sdk_03_03_00_03\packages\ti\drivers\canfd\test\xwr68xx"
And the "testSelection" choose "5" and it shows the EVM board is in transmit mode.
But I still can not receive any CAN-FD signal on oscilloscope or pcan.
Please help to solve this problem A.S.A.P.
BR
Thanks
Frank