Part Number: AM3359
Tool/software: Code Composer Studio
HI, I'd like to Debug and Control the GPIO on the AM3359 with CCS 9.1.0
Below is what I do:
1. Create the new Target configuration
2. Choose the connection as the picture shows
3. Test the connection, and it shows connect successfully
4. Launch the Configuration
And when I right click on the CortxA8 and choose connect target, it shows nothing.
And if I right click on the M3_wakeupSS and choose connect target, it shows the error message
I wonder which step I did is wrong, or if I want to control the GPIO by CCS, what should I do.