This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/LAUNCHXL-CC2640R2: OAD flash error after add a new task in Simple_Peripheral

Part Number: LAUNCHXL-CC2640R2


Tool/software: Code Composer Studio

Hi,

I'm trying to add a new task in simple_peripheral_oad_offchip example to control LED at differente BLE connection status, using mailbox to pass command.

But after add this task, the OAD will fail and return OAD_FLASH_ERROR.

Is there anyway to check the problem?

Using CCS the latest version and SDK version is simplelink_cc2640r2_sdk_3_20_00_21.

If there is more information need to provide, please let me know.

BTW, I tried to add uartlog to simple_peripheral example, and it will become very hard to discover UUID by btool, also, the OAD process will timeout at the first WriteImageBlock.

Is there conflict between uartlog and the example?

Thanks.