This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS570LS3137: I am following the below links but with no sucess to update my BRICKED XDS 200.

  • Hi,

    If you tested it on a different host, checked if the xds2xx_conf utility cannot detect the Debug Probe and you are sure the device drivers are properly installed, then I would try the methods shown in the section Re-flash the firmware of onboard XDS200 units of the XDS200 page you sent before. 

    If you had done this, then I would strongly suspect the probe itself is damaged. 

    Just one last detail: I just want to be sure you are not trying to connect to the built-in Debug Probe to the TMDS570LS31HDK - it uses a XDS100v2 instead. 

    Hope this helps,

    Rafael