Part Number: TMS320F280049C
Other Parts Discussed in Thread: C2000WARE
Tool/software: Code Composer Studio
Hi,
I am new to CCS and TI controllers.
I've read documentation for a few days now and want to start a new project (in stead of copying another project and change).
I managed to start a new project (use the project wizard), got the debugger working, C20000WARE is included (2.01), but:
1) when I include driverlib.lib I et errors like: #1965 cannot open source file "driverlib.lib" (it is also not in the project, like othe examples - ho to add?)
2) I do not have the \device folder with device.c/.h, f28004x_codestartbranch.asm etc.
Above does excist in eg. the example "receiver" project, supplied withC2000WARE.
Most important is: where to find this kind of documentation? (i did read the getting started etc etc etc, so please point it out)
Kind regards,
Ruud