Part Number: MSP430FR2355
Other Parts Discussed in Thread: CCSTUDIO, CODECOMPOSER
Tool/software: Code Composer Studio
So I just installed code composer 9 on my linux system and I'm having a very annoying issue. I can't seem to figure out how to launch the application.
I didn't have it create a desktop icon, as I'm not a fan of them. I couldnt figure a command line call to launch it. tried ccs, codecomposer, ccstudio, etc. Did some searching and found the executable in /ti/ccs930/eclipse which was ccstudio. I can launch that with ./ccstudio. However, it doesn't allow me to pin it to the favorites bar and I have to be in that directory to launch it.
How do I generate a command line executable that I can launch from anywhere, that will allow me to pin it to the favorites.
Should I simply create an alias in bashrc or is there something else I should do ?