Part Number: TM4C129ENCPDT
Tool/software: TI C/C++ Compiler
Hi All,
How to use Zlib library with tirtos? I need compression and decompression.
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TM4C129ENCPDT
Tool/software: TI C/C++ Compiler
Hi All,
How to use Zlib library with tirtos? I need compression and decompression.
Thanks
Hi Todd, I tried to add an external library (zlib) to the project but getting the linking error.
I added -
C:\zlibz\zlib-1.2.3-lib\include to the compiler include path
C:\zlibz\zlib-1.2.3-lib\lib\libz.a to the linker library path
C:\zlibz\zlib-1.2.3-lib\lib\ to the linker directory search.
But, during the linking time, I am getting unresolved symbols.
The same thing I did into CodeBlocks and everything works fine. It seems like CCS is not picking up the libz.a file somehow. Do you have any idea??
Thanks
Are you using the TI or GCC compiler tools?
Can you confirm by looking at the CCS build console that the library is actually getting passed to the linker? If you attach the complete build log that might help us identify where the issue might be.