Tool/software: Code Composer Studio
After a fresh install of CCS 10.0.0.00010 under Ubuntu 18.04.4 LTS attempted to install ti_cgt_c2000_18.1.1.LTS.
CCS 10 downloaded the installer, and after selected to re-start to complete the installation CCS didn't restart successfully. Attempting to run ccstudio from the command line cause the splash screen to appear, but ccsstudio just exited without reporting any obvious error before got to the dialogue where you select the workspace.
The contents of the eclipse/downloads directory was the following:
$ ls ~/ti/ccs1000/ccs/eclipse/downloads/ ccs_update_10.0.0.00010.run ccs_update_5.5.0.00092.bin com.ti.cgt.c2000.17.linux_manifest.xml com.ti.cgt.c2000.17.linux.properties startupInstaller_6.0.0.201611291427.log ti_cgt_c2000_18.1.1.LTS_linux_installer_x86.bin
The startupInstaller_6.0.0.201611291427.log file contained the following, for every failed attempt to start ccstudio:
Logging on 2020/03/21 19:32:00 2020-03-21 19:32:00.793: copying ccs_update_5.5.0.00092.bin 2020-03-21 19:32:00.793: in copyFiles, copying utils to downloads 2020-03-21 19:32:00.796: copyFile: /home/mr_halfword/ti/ccs1000/ccs/eclipse/utils/ccs_update_5.5.0.00092.bin to /home/mr_halfword/ti/ccs1000/ccs/eclipse/downloads/ccs_update_5.5.0.00092.bin 2020-03-21 19:32:00.801: copying ccs_update_10.0.0.00010.run 2020-03-21 19:32:00.801: in copyFiles, copying utils to downloads 2020-03-21 19:32:00.801: copyFile: /home/mr_halfword/ti/ccs1000/ccs/eclipse/utils/ccs_update_10.0.0.00010.run to /home/mr_halfword/ti/ccs1000/ccs/eclipse/downloads/ccs_update_10.0.0.00010.run SI_MAIN: higestfile = ccs_update_5.5.0.00092.bin SI_MAIN: utilFile = ccs_update_5.5.0.00092.bin highest file is not null SI_Main: Find file to run /home/mr_halfword/ti/ccs1000/ccs/eclipse/downloads/ccs_update_5.5.0.00092.bin SI_Main: exec cmdargs[0] /home/mr_halfword/ti/ccs1000/ccs/eclipse/downloads/ccs_update_5.5.0.00092.bin SI_Main: exec cmdargs[1] --ccs SI_Main: exec cmdargs[2] true SI_Main: exit code 0
Searching for the "highest file is not null" message found the related thread, for which got the idea to run the ccs_update_10.0.0.00010.run executable in the eclipse/downloads directory. When ccs_update_10.0.0.00010.run was manually run from the command line the ti_cgt_c2000_18.1.1.LTS installer was run and then CCS successfully started, and the new compiler was available and could be used.
Is this a issue with CCS 10 or the compiler installer?