Part Number: TMS320C6747
Tool/software: TI C/C++ Compiler
Hi y'all,
I've successfully migrated my project from CCS v3.3, to v5.2, then to v9.1.0. However, now in v9.1.0 I'm getting the following warnings of incompatibility. I don't want to ignore them, I want to use compatible tools. So, how can I determine the latest version of the combination of DSP/BIOS and compiler that I can use? I also show my versions in the table below. I cannot go any newer than 7.4.23 since I need to support COFF ABI. I suppose I can revert back to my CCS v5.2 versions, but I'd rather move to newer versions.
warning #16002-D: build attribute vendor section TI missing in
"C:/ti/ccs910/bios_5_42_02_10/packages/ti/bios/lib/bios.a64P<biosdata.o64P>"
: compatibility cannot be determined
CCS DSP/BIOS Version Code Gen Tools (compiler) XDAIS
CCS v3.3 5.33.06 6.1.23 ?
CCS v5.2 5.41.13.42 7.3.4 7.21.01.07
CCS v9.1.0 5.42.02.10 7.4.23 7.24.00.04 (BIOS / compiler not compatible)
Thank you so much and be safe!
Dave