Part Number: TMS320F28379D
Tool/software: Code Composer Studio
hi,
I am going through lab5 "System Initialization" from TMS320F2837xD micro-controller Workshop and I got the Below ERROR after i clicked the "build" Bottom. Can you please tell me how to fix these errors:
1) Description Resource Path Location Type
#1965 cannot open source file "F2837xD_device.h" F2837xD_GlobalVariableDefs.c /Lab5 line 43 C/C++ Problem
2) Description Resource Path Location Type
#1965 cannot open source file "Lab.h" Gpio.c /Lab5 line 7 C/C++ Problem
3) C28xx_CPU1: GEL Output:
Memory Map Initialization Complete
C28xx_CPU1: If erase/program (E/P) operation is being done on one core, the other core should not execute from shared-RAM (SR) as they are used for the E/P code. Also, CPU1 will be halted to determine SR ownership for the CPU which will run the Flash Plugin code, after which CPU1 will be set to run its application. User code execution from SR could commence after both flash banks are programmed.
C28xx_CPU1: GEL: Encountered a problem loading file: C:\C28x\Labs\Lab5\cpu01\Debug\Lab5.out Could not open file
thank you