This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS: !ERROR: No valid Eclipse project can be found at location



Tool/software: Code Composer Studio

Hi, unable to import CCS project through eclipsec for headless build. Using code composer studio v. 9.2. Works fine with ccs IDE, but need to do headless build. Used Command Prompt. Windows 10 64bit. Followed this documentation: 
http://software-dl.ti.com/ccs/esd/documents/ccs_projects-command-line.html#overview

Command used: 

eclipsec -noSplash -data C:\workspace\_ws-ccs\ -application com.ti.ccstudio.apps.projectImport -ccs.location C:\workspace\_project\TI\C4\

LOG:



!SESSION 2020-03-26 10:42:36.044 ----------------------------------------------- eclipse.buildId=4.8.0.I20180611-0500 java.version=1.8.0_144 java.vendor=Oracle Corporation BootLoader constants: OS=win32, ARCH=x86_64, WS=win32, NL=en_US Framework arguments: -application com.ti.ccstudio.apps.projectImport -ccs.location C:\workspace\_project\TI\C4\ Command-line arguments: -os win32 -ws win32 -arch x86_64 -data C:\workspace\_ws-ccs\ -application com.ti.ccstudio.apps.projectImport -ccs.location C:\workspace\_project\TI\C4\ !ENTRY com.ti.common.core 1 0 2020-03-26 10:42:38.817 !MESSAGE path=ccs_base/DebugServer !ENTRY com.ti.common.core 1 0 2020-03-26 10:42:38.826 !MESSAGE debugServerDir=C:/ti/ccs920/ccs/ccs_base/DebugServer