This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

编译器/ TDA2P-ACD:Relevant basic information for help--- TDA2P-ACD

Part Number: TDA2P-ACD


Tool/software: TI C / C ++编译器

I have only recently started using TI chips, and I use the Windows environment for development.
Which tool is used to configure the chip's clock?
How to associate the SDK, PinMux and TI_RTOS c code in the project?

I want to use the chip to debug the underlying drivers such as CAN, SPI, I2C, etc.


If you have some information or suggestions, please tell me, thank you!

 

  • Hi,

    you need to download VisionSDK for TDAxx devices:

    When install it you can check documentation in "PROCESSOR_SDK_VISION_03_08_00_00\vision_sdk\docs" folder to get familiar with the SDK.

    As part of VisionSDK it includes PDK (Platform Development Kit), which contains the drivers and test applications for various peripherals, you can check documentation here:

    Also you may find this trainings useful:


     


     


     

    Hope this helps.

    Regards,

    Yordan