Part Number: MSP432P401R
Tool/software: Code Composer Studio
hi,
i am using msp432p401r(TI-RTOS).
sdk simplelink_msp432p4_sdk_3_30_00_13
-I want to increase Idle Task Stack Size,how do i do this ?
There is no .cfg file in the project
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: MSP432P401R
Tool/software: Code Composer Studio
hi,
i am using msp432p401r(TI-RTOS).
sdk simplelink_msp432p4_sdk_3_30_00_13
-I want to increase Idle Task Stack Size,how do i do this ?
There is no .cfg file in the project
Hi Sinan,
I found that example project. This is a uart driver project. When you import and build it, a default kernel configuration project is automatically imported and built first, then your project. You will find the release.cfg file there.
* When building in Code Composer Studio, the kernel configuration project will
be imported along with the example. The kernel configuration project is
referenced by the example, so it will be built first. The "release" kernel
configuration is the default project used. It has many debug features disabled.
These feature include assert checking, logging and runtime stack checks. For a
detailed difference between the "release" and "debug" kernel configurations and
how to switch between them, please refer to the SimpleLink MCU SDK User's
Guide. The "release" and "debug" kernel configuration projects can be found
under <SDK_INSTALL_DIR>/kernel/tirtos/builds/<BOARD>/(release|debug)/(ccs|gcc).