Part Number: IWR6843
Tool/software: Code Composer Studio
I modified the source code and want to generate a bin file but my bin file after modified can't use with GUI.
My PC's OS is Windows 10.
My device is ES2.
Code Composer Studio 8.3.1
mmwave_sdk_03_03_00_03
mmwave_industrial_toolbox_4_2_1
As I know, after modification, we need to setup the build environment. I checked setenv.bat, its path is correct.
@REM ############################################################################### @REM # @REM # Set up tools and build environment variables for mmwave sdk @REM # @REM ############################################################################### @REM ############################################################################### @REM # Build variables (to be modified based on build need) @REM ############################################################################### @REM Select your device. Options (case sensitive) are: awr14xx, iwr14xx, awr16xx, iwr16xx, awr18xx, iwr18xx, iwr68xx set MMWAVE_SDK_DEVICE=iwr68xx @REM If download via CCS is needed, set below define to yes else no @REM yes: Out file created can be loaded using CCS. @REM Binary file created can be used to flash @REM no: Out file created cannot be loaded using CCS. @REM Binary file created can be used to flash @REM (additional features: write-protect of TCMA, etc) set DOWNLOAD_FROM_CCS=yes @REM If using a secure device this variable needs to be updated with the path to mmwave_secdev_<ver> folder set MMWAVE_SECDEV_INSTALL_PATH= @REM If using a secure device, this variable needs to be updated with the path to hsimage.cfg file that @REM has customer specific certificate/key information. A sample hsimage.cfg file is in the secdev package set MMWAVE_SECDEV_HSIMAGE_CFG=%MMWAVE_SECDEV_INSTALL_PATH%/hs_image_creator/hsimage.cfg @REM ############################################################################### @REM # Customer installed tools variables (to be modified based on the installation) @REM ############################################################################### @REM ############################################################################### @REM # TI tools variables (no changes needed below this line if default mmwave sdk @REM # installation options are used) @REM ############################################################################### set MMWAVE_SDK_TOOLS_INSTALL_PATH=C:/ti @REM Common settings for all platforms @REM Path to <mmwave_sdk installation path>/packages folder set MMWAVE_SDK_INSTALL_PATH=%MMWAVE_SDK_TOOLS_INSTALL_PATH%/mmwave_sdk_03_03_00_03/packages @REM TI ARM compiler set R4F_CODEGEN_INSTALL_PATH=%MMWAVE_SDK_TOOLS_INSTALL_PATH%/ti-cgt-arm_16.9.6.LTS @REM TI XDC TOOLS set XDC_INSTALL_PATH=%MMWAVE_SDK_TOOLS_INSTALL_PATH%/xdctools_3_50_08_24_core @REM TI BIOS set BIOS_INSTALL_PATH=%MMWAVE_SDK_TOOLS_INSTALL_PATH%/bios_6_73_01_01/packages @REM awr14xx/iwr14xx radarss firmware set XWR14XX_RADARSS_IMAGE_BIN=%MMWAVE_SDK_INSTALL_PATH%/../firmware/radarss/xwr12xx_xwr14xx_radarss_rprc.bin @REM awr16xx/iwr16xx radarss firmware set XWR16XX_RADARSS_IMAGE_BIN=%MMWAVE_SDK_INSTALL_PATH%/../firmware/radarss/xwr16xx_radarss_rprc.bin @REM awr18xx/iwr18xx radarss firmware set XWR18XX_RADARSS_IMAGE_BIN=%MMWAVE_SDK_INSTALL_PATH%/../firmware/radarss/xwr18xx_radarss_rprc.bin @REM iwr68xx radarss firmware set XWR68XX_RADARSS_IMAGE_BIN=%MMWAVE_SDK_INSTALL_PATH%/../firmware/radarss/iwr6xxx_radarss_rprc.bin @REM Following only needed for devices with DSP @REM TI DSP compiler set C674_CODEGEN_INSTALL_PATH=%MMWAVE_SDK_TOOLS_INSTALL_PATH%/ti-cgt-c6000_8.3.3 @REM DSPlib set C64Px_DSPLIB_INSTALL_PATH=%MMWAVE_SDK_TOOLS_INSTALL_PATH%/dsplib_c64Px_3_4_0_0 @REM DSPlib C674 set C674x_DSPLIB_INSTALL_PATH=%MMWAVE_SDK_TOOLS_INSTALL_PATH%/dsplib_c674x_3_4_0_0 @REM MATHlib set C674x_MATHLIB_INSTALL_PATH=%MMWAVE_SDK_TOOLS_INSTALL_PATH%/mathlib_c674x_3_1_2_1 @REM Call script to check env variables and set paths call checkenv.bat @REM Check error code IF %ERRORLEVEL% NEQ 0 ( REM ERROR: Failure in checkenv.bat !!! REM Return error EXIT /B 1 ) EXIT /B 0
Then I checked the method to build demo in windows
REM Fill <device type> with appropriate device that supports demo in a particular release cd %MMWAVE_SDK_INSTALL_PATH%/ti/demo/<device type>/mmw REM Clean and build gmake clean gmake all REM Incremental build gmake all REM For example to build the mmw demo for iwr68xx cd %MMWAVE_SDK_INSTALL_PATH%/ti/demo/xwr68xx/mmw gmake clean gmake all REM This will create xwr68xx_mmw_demo_mss.xer4f & xwr68xx_mmw_demo.bin binaries REM under %MMWAVE_SDK_INSTALL_PATH%/ti/demo/xwr68xx/mmw folder
I can't run these commands on Windows cmd. It said: "gmake is not recognized as an internal or external command". Even though I checked my Gmake version is 4.1 in the path C:\ti\ccsv8\utils\bin
How to generate bin file that can work with GUI normally in this case?