Part Number: TMS320C5504
Other Parts Discussed in Thread: OMAP5912
Tool/software: TI C/C++ Compiler
The project generates a binary that is placed into the DSP on an OMAP5912. This project was previously built on Code Composer v3.3 and I am attempting to update the project to be built on a more modern version. The project builds with only a handful of warnings, but the binary does not function. I have tried finding a download for the previous version of the tools, but they are obsolete. The release notes for even 4.0.0 are removed, so I cannot find documentation for the changes.
Are there any resources or perhaps a download for the older tool that I can be directed to?
Previous C55x tools were version 3.3.2, the newer tools are version 4.4.1.