Part Number: CCSTUDIO
Other Parts Discussed in Thread: C2000WARE
Tool/software: Code Composer Studio
On a Windows 10 machine I installed Code Composer 9.3 along with the packages C2000Ware_3_01_00_00 and C2000Ware_2_01_00_00. However, Code Composer would not recognize either C2000Ware package. I verified this in Code Composer by selecting the menu item "Window" then navigating Preferences->Code Composer Studio->Products. Under "Installed Products" XDCtools was listed but not C2000Ware. I tried adding the following directories to the "Product discovery path"
C:\ti\c2000
C:\ti\c2000\C2000Ware_2_01_00_00
C:\ti\c2000\C2000Ware_3_01_00_00
and then I selected "Refresh" but nothing showed up in the installed products.
So I found the post
who said they fixed it "by renaming "metadata/tirex" at the root of the C2000Ware installation as ".metadata/.tirex" "
So I checked both C:\ti\c2000\C2000Ware_2_01_00_00 and C:\ti\c2000\C2000Ware_3_01_00_00. Both of their metadata/tirex did not have the leading period. So I also renamed the directories and code composer recognized both in the installed products. I then checked another computer which works and it also had the leading period.
Why is are the installers for C2000Ware failing to correctly name the metadata directory and breaking code composer?
Thanks, Paul