Other Parts Discussed in Thread: IWR6843, AWR1843, AWR1642
Tool/software: Code Composer Studio
Hi guys,
I am making some application with your radar sensors. I have tried to port the code from AWR1843 to IWR6843, and the code builds and runs on the system, but there are some issues. The main issue is that after I load the cfg over UART, and dss subsystem starts initiating datapath, i get this console output:
Error: MMWDemoDSS mmWave Start failed [Error code -204602898]
Debug: MMWDemoDSS Data Path start failed with Error[-1]
Debug: MMWDemoDSS Data path exit
At the moment, i have no idea how to understand an error code, is there some description in your documentation about error codes? If there is, could you give me some instructions on how to find it?
Kind regards,
Aleksa