This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS320F28388D: tmdxiddk379d

Part Number: TMS320F28388D

Tool/software: Code Composer Studio

I'm trying to do "6 Incremental build level 1" in "Quick Response Control of PMSM Using Fast Current Loop".

In "Figure 5.", the state of rumMotor is "MOTOR_RUN".

Originally the value  of "runMotor" in example code is "MOTOR_STOP".

So I tried to change from "MOTOR_STOP" to "MOTOR_RUN" during debugging mode.

But, the state was not changed.

everytime I tried to change the state, I failed.

Is there some special setting?

Please let me know.

thank you.