I'm just getting started with my MSP430 LaunchPad and quickly ran into a problem which others have had. I tried to resolve the problem as suggested in other posts, but still end up with the same error message:
Code composer starts up fine, with the title bar of the window saying I have a "(Licensed)" version. I enter a .c program which compiles without errors, but when I try to debug the program, the title bar changes to "(Unlicensed)" and I am prompted to register or specify a license file or license server. When I specify the .lic file I received from TI, I get the error shown on the image attached.
I have only one .lic file C:\Program Files (x86)\Texas Instruments\ccsv4\DebugServer\license\TMDSCCS-HWN01A-v4.0.lic
Any suggestions would be appreciated.
Thanks in advance,
Gertrude