This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/CC3220MODA: Interfacing assembly with c/c++

Part Number: CC3220MODA

Tool/software: Code Composer Studio

This should be simple but I cannot seem to find the answer; I am optimizing a bit of c/c++ code with assembly and need to interface with a few global variables declared on the c/c++ side. I cant seem to find how to do this. So for example:

==== c/c++ side defines these variables

int globalVar;

int globalArray[10];

=====

.global myfunc

myfunc;

ldr  r0, <value of globalVar>

ldr  r1, <address of globaVar>

ldr  r2, <address of globalArray>

With the stuff between brackets <> what I don't know.  I have the "ARMAssemblyLanguageToolsv18.1.0.LTS" from 2018 doc but this is either not documenting it or I missed it.