Hi, I've installed the ccsv4 but when I try connecting it to the ezdsp f28335 it says that the license is not installed. What sort of license do I need to use to create projects for the f28335. I had the original ccs v3 Cd that came with the package but unfortunately it broke. Will installing the license enable indefinite use of the ccsv4 and the f28335 without code size limitations and subscriptions or will there restrictions?
I have read through the 'getting started with ccsv4' wiki but it does't say anything about licensing issues. How can I enable the fully functionalality of the ccs for f28335 similar to the CD version that came in the box?