This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Anyone know what this error code means? I can no longer connect to my F28335

Two of my prototype boards have stopped working.  I can no longer connect in debug mode.  

Here's the error from the console:

C28xx: Error connecting to the target: Error 0x80000240/-230 Fatal Error during: Initialization, OCS,  

C28xx: Error connecting to the target: Error 0x80000200/-1047 Fatal Error during: OCS,  PTI_ERR_EMU_CLOSE Error Occured at 0x00000000 

I notice that the DSC is toggling the XRS line too.  

I'm not sure what caused them to get to this state.  I was trouble shooting a hardware problem that may have brought down either the 3.3V or 1.8V rails temporarily.

Is there some way to bring these back to life?  These delfinos seem to be very difficult to get and I don't have any spares.  

Any help would be appreciated.  Thanks