This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Passing arguments to assembly statements in C

I don't see a way to do this, but I'll ask:

Is there a way to pass arguments to inline assembly statements, ala gcc?  If so, how?

Thanks,

Matt

  • No.  But consider using intrinsics instead.  Intrinsics act like function calls, but are (with a few exceptions) implemented with a single instruction.

    Thanks and regards,

    -George

  • That is not supported by the TI inline assembly syntax.

  • This seems like an odd reply, since it is unstated that the function I wish to implement is one that's already defined.  I wish to read a co-processor register in C, and put it somewhere, like gcc would allow me to do.

  • The usual method in TI C code is with a cregister, reading a memory-mapped location, or using an assembly code helper function

    On C6x, to read the CSR register, you could do:

    #include <c6x.h>
    unsigned int csr_val = CSR;

    However, the names of coprocessor registers aren't usually built in to the compiler and assembler.  How would you have named this coprocessor register if you could have used gcc-style inline assembly?  Is there a built-in name for it already, or would you have used its address?

    Suppose it's memory mapped:

    #define LOCATION 0x12345678
    unsigned int value = *((volatile unsigned int *)LOCATION);

    Obviously calling an assembly code helper function has the call/return overhead