Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS320F28379D: Memory map prevented reading a mapped hardware register.

Part Number: TMS320F28379D
Other Parts Discussed in Thread: C2000WARE

Tool/software: Code Composer Studio

When debugging our LaunchXL-F2379D through the onboard XDS100we cannot see registers associated with a hardware peripheral, though the data pointers can be seen pointing to the correct addresses in memory to do so. This only occurs within implementations where we utilize CAN, and is isolated to this module as well. Similar operations on other peripherals like SCI and CPU Timers yields expected behavior. With the CAN register sets, however, not only are reads unavailable to us within the debugger view (seen in the picture below, reads to the pointer 'm_Reg' at the lowest level return an error), we also cannot seem to update the registers from compiled instruction sets as we watch them in real time from within the register window. As we make direct writes to the pointer 'm_Reg' mentioned above, the values are not reflected as they should be within the hardware registers. I have included our linker command file as well.

Attempting to look at the registers through our variable window is the best clue that we've been able to find so far. Expanding the data pointer which is meant to point at the register its wrapper class is named after tells us that the "memory map prevented reading address ... " though looking at the pointer itself, we see that it is indeed pointing at the location it is meant to. The CAN register section is separate from the other peripherals in location and function, so I think that we are missing some rule or statement that configures either the compiled code or the debugger to read them correctly.

The memory sections defined there map to the correct locations for this microprocessor, and our source code references those sections using "#pragma DATA_SECTION()". I have included the linker file and our register definition file, they are the default C2000Ware provided versions with some modifications made. I am not able to provide source code, but if there is any other forms of data that would be helpful then I am happy to provide them.

MEMORY
{
PAGE 0 :  /* Program Memory */
          /* Memory (RAM/FLASH) blocks can be moved to PAGE1 for data allocation */
          /* BEGIN is used for the "boot to Flash" bootloader mode   */

   BEGIN           	: origin = 0x080000, length = 0x000002
   RAMM0           	: origin = 0x000122, length = 0x0002DE
   RAMD0           	: origin = 0x00B000, length = 0x000800
   RAMLS0          	: origin = 0x008000, length = 0x000800
   RAMLS1          	: origin = 0x008800, length = 0x000800
   RAMLS2      		: origin = 0x009000, length = 0x000800
   RAMLS3      		: origin = 0x009800, length = 0x000800
   RAMLS4      		: origin = 0x00A000, length = 0x000800
   RAMGS14          : origin = 0x01A000, length = 0x001000     /* Only Available on F28379D, F28377D, F28375D devices. Remove line on other devices. */
   RAMGS15          : origin = 0x01B000, length = 0x001000     /* Only Available on F28379D, F28377D, F28375D devices. Remove line on other devices. */
   RESET           	: origin = 0x3FFFC0, length = 0x000002

   /* Flash sectors */
   FLASHA           : origin = 0x080002, length = 0x001FFE	/* on-chip Flash */
 /*FLASHB           : origin = 0x082000, length = 0x002000	/* on-chip Flash */
   FLASHBC          : origin = 0x082000, length = 0x004000	/* on-chip Flash */
   FLASHD           : origin = 0x086000, length = 0x002000	/* on-chip Flash */
 /*FLASHE           : origin = 0x088000, length = 0x008000	/* on-chip Flash */
 /*FLASHF       	: origin = 0x090000, length = 0x008000	/* on-chip Flash */
 /*FLASHG           : origin = 0x098000, length = 0x008000	/* on-chip Flash */
 /*FLASHH           : origin = 0x0A0000, length = 0x008000	/* on-chip Flash */
 /*FLASHI           : origin = 0x0A8000, length = 0x008000	/* on-chip Flash */
   FLASHEFGHIJ      : origin = 0x088000, length = 0x030000	/* on-chip Flash */
 /*FLASHK           : origin = 0x0B8000, length = 0x002000	/* on-chip Flash */
 /*FLASHL           : origin = 0x0BA000, length = 0x002000	/* on-chip Flash */
 /*FLASHM           : origin = 0x0BC000, length = 0x002000	/* on-chip Flash */
   FLASHKLMN        : origin = 0x0B8000, length = 0x008000	/* on-chip Flash */

PAGE 1 : /* Data Memory */
         /* Memory (RAM/FLASH) blocks can be moved to PAGE0 for program allocation */

   BOOT_RSVD       : origin = 0x000002, length = 0x000120     /* Part of M0, BOOT rom will use this for stack */
   RAMM1           : origin = 0x000400, length = 0x000400     /* on-chip RAM block M1 */
   RAMD1           : origin = 0x00B800, length = 0x000800

   RAMLS5      : origin = 0x00A800, length = 0x000800

   RAMGS0      : origin = 0x00C000, length = 0x001000
   RAMGS1      : origin = 0x00D000, length = 0x001000
   RAMGS2      : origin = 0x00E000, length = 0x001000
   RAMGS3      : origin = 0x00F000, length = 0x001000
   RAMGS4  	   : origin = 0x010000, length = 0x001000
 /*RAMGS5      : origin = 0x011000, length = 0x001000
   RAMGS6      : origin = 0x012000, length = 0x001000
   RAMGS7      : origin = 0x013000, length = 0x001000
   RAMGS8      : origin = 0x014000, length = 0x001000*/
   RAMGS56789  : origin = 0x011000, length = 0x005000
   RAMGS10     : origin = 0x016000, length = 0x001000
   RAMGS11     : origin = 0x017000, length = 0x001000
   RAMGS12     : origin = 0x018000, length = 0x001000     /* Only Available on F28379D, F28377D, F28375D devices. Remove line on other devices. */
   RAMGS13     : origin = 0x019000, length = 0x001000     /* Only Available on F28379D, F28377D, F28375D devices. Remove line on other devices. */

   CPU2TOCPU1RAM   : origin = 0x03F800, length = 0x000400
   CPU1TOCPU2RAM   : origin = 0x03FC00, length = 0x000400

   ADCA_RESULT   : origin = 0x000B00, length = 0x000020
   ADCB_RESULT   : origin = 0x000B20, length = 0x000020
   ADCC_RESULT   : origin = 0x000B40, length = 0x000020
   ADCD_RESULT   : origin = 0x000B60, length = 0x000020

   ADCA          : origin = 0x007400, length = 0x000080
   ADCB          : origin = 0x007480, length = 0x000080
   ADCC          : origin = 0x007500, length = 0x000080
   ADCD          : origin = 0x007580, length = 0x000080

   ANALOG_SUBSYS : origin = 0x05D180, length = 0x000080

   CANA          : origin = 0x048000, length = 0x000800
   CANB          : origin = 0x04A000, length = 0x000800

   CLA1          : origin = 0x001400, length = 0x000040     /* CLA registers */

   CLB_XBAR      : origin = 0x007A40, length = 0x000040

   CMPSS1        : origin = 0x005C80, length = 0x000020
   CMPSS2        : origin = 0x005CA0, length = 0x000020
   CMPSS3        : origin = 0x005CC0, length = 0x000020
   CMPSS4        : origin = 0x005CE0, length = 0x000020
   CMPSS5        : origin = 0x005D00, length = 0x000020
   CMPSS6        : origin = 0x005D20, length = 0x000020
   CMPSS7        : origin = 0x005D40, length = 0x000020
   CMPSS8        : origin = 0x005D60, length = 0x000020

   CPU_TIMER0    : origin = 0x000C00, length = 0x000008     /* CPU Timer0 registers */
   CPU_TIMER1    : origin = 0x000C08, length = 0x000008     /* CPU Timer1 registers */
   CPU_TIMER2    : origin = 0x000C10, length = 0x000008     /* CPU Timer2 registers */

   DACA          : origin = 0x005C00, length = 0x000010
   DACB          : origin = 0x005C10, length = 0x000010
   DACC          : origin = 0x005C20, length = 0x000010

   DMA          : origin = 0x001000, length = 0x000200
   DMACLASRCSEL : origin = 0x007980, length = 0x000040

   ECAP1        : origin = 0x005000, length = 0x000020     /* Enhanced Capture 1 registers */
   ECAP2        : origin = 0x005020, length = 0x000020     /* Enhanced Capture 2 registers */
   ECAP3        : origin = 0x005040, length = 0x000020     /* Enhanced Capture 3 registers */
   ECAP4        : origin = 0x005060, length = 0x000020     /* Enhanced Capture 4 registers */
   ECAP5        : origin = 0x005080, length = 0x000020     /* Enhanced Capture 5 registers */
   ECAP6        : origin = 0x0050A0, length = 0x000020     /* Enhanced Capture 6 registers */

   EMIF1        : origin = 0x047000, length = 0x000800
   EMIF2        : origin = 0x047800, length = 0x000800

   EQEP1        : origin = 0x005100, length = 0x000040     /* Enhanced QEP 1 registers */
   EQEP2        : origin = 0x005140, length = 0x000040     /* Enhanced QEP 2 registers */
   EQEP3        : origin = 0x005180, length = 0x000040     /* Enhanced QEP 3 registers */

   EPWM1        : origin = 0x004000, length = 0x000100     /* Enhanced PWM 1 registers */
   EPWM2        : origin = 0x004100, length = 0x000100     /* Enhanced PWM 2 registers */
   EPWM3        : origin = 0x004200, length = 0x000100     /* Enhanced PWM 3 registers */
   EPWM4        : origin = 0x004300, length = 0x000100     /* Enhanced PWM 4 registers */
   EPWM5        : origin = 0x004400, length = 0x000100     /* Enhanced PWM 5 registers */
   EPWM6        : origin = 0x004500, length = 0x000100     /* Enhanced PWM 6 registers */
   EPWM7        : origin = 0x004600, length = 0x000100     /* Enhanced PWM 7 registers */
   EPWM8        : origin = 0x004700, length = 0x000100     /* Enhanced PWM 8 registers */
   EPWM9        : origin = 0x004800, length = 0x000100     /* Enhanced PWM 9 registers */
   EPWM10       : origin = 0x004900, length = 0x000100     /* Enhanced PWM 10 registers */
   EPWM11       : origin = 0x004A00, length = 0x000100     /* Enhanced PWM 11 registers */
   EPWM12       : origin = 0x004B00, length = 0x000100     /* Enhanced PWM 12 registers */

   EPWM_XBAR    : origin = 0x007A00, length = 0x000040

   FLASH0_CTRL  : origin = 0x05F800, length = 0x000300
   FLASH0_ECC   : origin = 0x05FB00, length = 0x000040

   GPIOCTRL     : origin = 0x007C00, length = 0x000180     /* GPIO control registers */
   GPIODAT      : origin = 0x007F00, length = 0x000030     /* GPIO data registers */

   OUTPUT_XBAR  : origin = 0x007A80, length = 0x000040
   I2CA         : origin = 0x007300, length = 0x000040     /* I2C-A registers */
   I2CB         : origin = 0x007340, length = 0x000040     /* I2C-B registers */

   IPC          : origin = 0x050000, length = 0x000024

   FLASHPUMPSEMAPHORE   : origin = 0x050024, length = 0x000002

   ROMPREFETCH  : origin = 0x05E608, length = 0x000002

   MEMCFG       : origin = 0x05F400, length = 0x000080     /* Mem Config registers */
   EMIF1CONFIG  : origin = 0x05F480, length = 0x000020     /* Emif-1 Config registers */
   EMIF2CONFIG  : origin = 0x05F4A0, length = 0x000020     /* Emif-2 Config registers */
   ACCESSPROTECTION  : origin = 0x05F4C0, length = 0x000040     /* Access Protection registers */
   MEMORYERROR  : origin = 0x05F500, length = 0x000040     /* Access Protection registers */
   ROMWAITSTATE : origin = 0x05F540, length = 0x000002     /* ROM Config registers */


   MCBSPA       : origin = 0x006000, length = 0x000040     /* McBSP-A registers */
   MCBSPB       : origin = 0x006040, length = 0x000040     /* McBSP-A registers */

   NMIINTRUPT   : origin = 0x007060, length = 0x000010     /* NMI Watchdog Interrupt Registers */

   PIE_CTRL     : origin = 0x000CE0, length = 0x000020     /* PIE control registers */
   PIE_VECT     : origin = 0x000D00, length = 0x000200     /* PIE Vector Table */
   SCIA         : origin = 0x007200, length = 0x000010     /* SCI-A registers */
   SCIB         : origin = 0x007210, length = 0x000010     /* SCI-B registers */
   SCIC         : origin = 0x007220, length = 0x000010     /* SCI-C registers */
   SCID         : origin = 0x007230, length = 0x000010     /* SCI-D registers */

   SDFM1        : origin = 0x005E00, length = 0x000080     /* Sigma delta 1 registers */
   SDFM2        : origin = 0x005E80, length = 0x000080     /* Sigma delta 2 registers */

   SPIA         : origin = 0x006100, length = 0x000010
   SPIB         : origin = 0x006110, length = 0x000010
   SPIC         : origin = 0x006120, length = 0x000010
   SPID         : origin = 0x006130, length = 0x000010

   UPP          : origin = 0x006200, length = 0x000100     /* uPP registers */

   DEV_CFG     : origin = 0x05D000, length = 0x000180
   CLK_CFG     : origin = 0x05D200, length = 0x000100
   CPU_SYS     : origin = 0x05D300, length = 0x000100

   INPUT_XBAR   : origin = 0x007900, length = 0x000020
   XBAR         : origin = 0x007920, length = 0x000020
   SYNC_SOC     : origin = 0x007940, length = 0x000010
   WD           : origin = 0x007000, length = 0x000040

   XINT         : origin = 0x007070, length = 0x000010

   DCSM_Z1      : origin = 0x05F000, length = 0x000030     /* Zone 1 Dual code security module registers */
   DCSM_Z2      : origin = 0x05F040, length = 0x000030     /* Zone 2 Dual code security module registers */
   DCSM_COMMON  : origin = 0x05F070, length = 0x000010     /* Common Dual code security module registers */
}

SECTIONS
{
   /* Allocate program areas: */
   .cinit              : >	FLASHBC,					PAGE = 0, ALIGN(4)
   .pinit              : >	FLASHBC,					PAGE = 0, ALIGN(4)
   .text               : >> FLASHEFGHIJ	| FLASHKLMN		PAGE = 0, ALIGN(4)
   codestart           : > 	BEGIN,     					PAGE = 0, ALIGN(4)

   /* Allocate uninitalized data sections: */
   .stack              : >	RAMD1,				PAGE = 1
   .ebss               : >	RAMGS56789,			PAGE = 1
   .esysmem            : > 	RAMGS3,				PAGE = 1
   .cio                : >> RAMGS3 | RAMGS4		PAGE = 1
   
   /* Initalized sections go in Flash */
   .econst             : > FLASHKLMN,      	PAGE = 0, ALIGN(4)
   .switch             : > FLASHKLMN,		PAGE = 0, ALIGN(4)

   .reset              : > RESET,     PAGE = 0, TYPE = DSECT /* not used, */

   Filter_RegsFile     : > RAMGS0,	   PAGE = 1

   SHARERAMGS0		: > RAMGS0,		PAGE = 1
   SHARERAMGS1		: > RAMGS1,		PAGE = 1
   ramgs0           : > RAMGS0,     PAGE = 1
   ramgs1           : > RAMGS1,     PAGE = 1

   UNION run = PIE_VECT, PAGE = 1
   {
      PieVectTableFile
      GROUP
      {
         EmuBModeVar
         EmuBootPinsVar
      }
   }

   AdcaResultFile        : > ADCA_RESULT,  PAGE = 1
   AdcbResultFile        : > ADCB_RESULT,  PAGE = 1
   AdccResultFile        : > ADCC_RESULT,  PAGE = 1
   AdcdResultFile        : > ADCD_RESULT,  PAGE = 1

   AdcaRegsFile          : > ADCA,         PAGE = 1
   AdcbRegsFile          : > ADCB,         PAGE = 1
   AdccRegsFile          : > ADCC,         PAGE = 1
   AdcdRegsFile          : > ADCD,         PAGE = 1

   AnalogSubsysRegsFile  : > ANALOG_SUBSYS, PAGE = 1

   CanaRegsFile          : > CANA,         PAGE = 1
   CanbRegsFile          : > CANB,         PAGE = 1

   Cla1RegsFile          : > CLA1,         PAGE = 1
   Cla1SoftIntRegsFile   : > PIE_CTRL,     PAGE = 1, type=DSECT

   ClbXbarRegsFile       : > CLB_XBAR     PAGE = 1

   Cmpss1RegsFile        : > CMPSS1,      PAGE = 1
   Cmpss2RegsFile        : > CMPSS2,      PAGE = 1
   Cmpss3RegsFile        : > CMPSS3,      PAGE = 1
   Cmpss4RegsFile        : > CMPSS4,      PAGE = 1
   Cmpss5RegsFile        : > CMPSS5,      PAGE = 1
   Cmpss6RegsFile        : > CMPSS6,      PAGE = 1
   Cmpss7RegsFile        : > CMPSS7,      PAGE = 1
   Cmpss8RegsFile        : > CMPSS8,      PAGE = 1

   CpuTimer0RegsFile     : > CPU_TIMER0,    PAGE = 1
   CpuTimer1RegsFile     : > CPU_TIMER1,    PAGE = 1
   CpuTimer2RegsFile     : > CPU_TIMER2,    PAGE = 1

   DacaRegsFile          : > DACA          PAGE = 1
   DacbRegsFile          : > DACB          PAGE = 1
   DaccRegsFile          : > DACC          PAGE = 1

   DcsmZ1RegsFile        : > DCSM_Z1,          PAGE = 1
   DcsmZ2RegsFile        : > DCSM_Z2,          PAGE = 1
   DcsmCommonRegsFile    : > DCSM_COMMON,      PAGE = 1

   DmaRegsFile           : > DMA           PAGE = 1
   DmaClaSrcSelRegsFile  : > DMACLASRCSEL  PAGE = 1

   ECap1RegsFile         : > ECAP1,        PAGE = 1
   ECap2RegsFile         : > ECAP2,        PAGE = 1
   ECap3RegsFile         : > ECAP3,        PAGE = 1
   ECap4RegsFile         : > ECAP4,        PAGE = 1
   ECap5RegsFile         : > ECAP5,        PAGE = 1
   ECap6RegsFile         : > ECAP6,        PAGE = 1

   Emif1RegsFile         : > EMIF1         PAGE = 1
   Emif2RegsFile         : > EMIF2         PAGE = 1

   EPwm1RegsFile         : > EPWM1,        PAGE = 1
   EPwm2RegsFile         : > EPWM2,        PAGE = 1
   EPwm3RegsFile         : > EPWM3,        PAGE = 1
   EPwm4RegsFile         : > EPWM4,        PAGE = 1
   EPwm5RegsFile         : > EPWM5,        PAGE = 1
   EPwm6RegsFile         : > EPWM6,        PAGE = 1
   EPwm7RegsFile         : > EPWM7,        PAGE = 1
   EPwm8RegsFile         : > EPWM8,        PAGE = 1
   EPwm9RegsFile         : > EPWM9,        PAGE = 1
   EPwm10RegsFile        : > EPWM10,       PAGE = 1
   EPwm11RegsFile        : > EPWM11,       PAGE = 1
   EPwm12RegsFile        : > EPWM12,       PAGE = 1

   EPwmXbarRegsFile      : > EPWM_XBAR     PAGE = 1

   EQep1RegsFile         : > EQEP1,        PAGE = 1
   EQep2RegsFile         : > EQEP2,        PAGE = 1
   EQep3RegsFile         : > EQEP3,        PAGE = 1

   Flash0CtrlRegsFile     : > FLASH0_CTRL    PAGE = 1
   Flash0EccRegsFile      : > FLASH0_ECC     PAGE = 1

   GpioCtrlRegsFile      : > GPIOCTRL,     PAGE = 1
   GpioDataRegsFile      : > GPIODAT,      PAGE = 1

   OutputXbarRegsFile    : > OUTPUT_XBAR    PAGE = 1
   I2caRegsFile          : > I2CA,          PAGE = 1
   I2cbRegsFile          : > I2CB,          PAGE = 1
   InputXbarRegsFile     : > INPUT_XBAR     PAGE = 1
   XbarRegsFile          : > XBAR           PAGE = 1
   IpcRegsFile           : > IPC,           PAGE = 1

   FlashPumpSemaphoreRegsFile   : > FLASHPUMPSEMAPHORE,    PAGE = 1

   RomPrefetchRegsFile       : > ROMPREFETCH,       PAGE = 1
   MemCfgRegsFile            : > MEMCFG,            PAGE = 1
   Emif1ConfigRegsFile       : > EMIF1CONFIG,       PAGE = 1
   Emif2ConfigRegsFile       : > EMIF2CONFIG,       PAGE = 1
   AccessProtectionRegsFile  : > ACCESSPROTECTION,  PAGE = 1
   MemoryErrorRegsFile       : > MEMORYERROR,       PAGE = 1
   RomWaitStateRegsFile      : > ROMWAITSTATE,      PAGE = 1

   McbspaRegsFile        : > MCBSPA,       PAGE = 1
   McbspbRegsFile        : > MCBSPB,       PAGE = 1

   UppRegsFile           : > UPP,          PAGE = 1

   NmiIntruptRegsFile    : > NMIINTRUPT,   PAGE = 1
   PieCtrlRegsFile       : > PIE_CTRL,     PAGE = 1

   SciaRegsFile          : > SCIA,         PAGE = 1
   ScibRegsFile          : > SCIB,         PAGE = 1
   ScicRegsFile          : > SCIC,         PAGE = 1
   ScidRegsFile          : > SCID,         PAGE = 1

   Sdfm1RegsFile         : > SDFM1,        PAGE = 1
   Sdfm2RegsFile         : > SDFM2,        PAGE = 1

   SpiaRegsFile          : > SPIA,        PAGE = 1
   SpibRegsFile          : > SPIB,        PAGE = 1
   SpicRegsFile          : > SPIC,        PAGE = 1
   SpidRegsFile          : > SPID,        PAGE = 1

   DevCfgRegsFile        : > DEV_CFG,     PAGE = 1
   ClkCfgRegsFile        : > CLK_CFG,     PAGE = 1
   CpuSysRegsFile        : > CPU_SYS,     PAGE = 1

   SyncSocRegsFile       : > SYNC_SOC,    PAGE = 1

   WdRegsFile            : > WD,           PAGE = 1

   XintRegsFile          : > XINT          PAGE = 1
   MemCfgRegs            : > MEMCFG        PAGE = 1

#ifdef __TI_COMPILER_VERSION__
	#if __TI_COMPILER_VERSION__ >= 15009000
	.TI.ramfunc : {}	LOAD = FLASHD,
						RUN = RAMLS0 | RAMLS1 | RAMLS2 |RAMLS3,
                  		LOAD_START(_RamfuncsLoadStart),
                     	LOAD_SIZE(_RamfuncsLoadSize),
                     	LOAD_END(_RamfuncsLoadEnd),
                      	RUN_START(_RamfuncsRunStart),
                       	RUN_SIZE(_RamfuncsRunSize),
                      	RUN_END(_RamfuncsRunEnd),
						PAGE = 0, ALIGN(4)
	#else
   ramfuncs            : LOAD = FLASHD,
                         RUN = RAMLS0 | RAMLS1 | RAMLS2 |RAMLS3,
                         LOAD_START(_RamfuncsLoadStart),
                         LOAD_SIZE(_RamfuncsLoadSize),
                         LOAD_END(_RamfuncsLoadEnd),
                         RUN_START(_RamfuncsRunStart),
                         RUN_SIZE(_RamfuncsRunSize),
                         RUN_END(_RamfuncsRunEnd),
                         PAGE = 0, ALIGN(4)    
    #endif
#endif

   /* The following section definitions are required when using the IPC API Drivers */
    GROUP : > CPU1TOCPU2RAM, PAGE = 1
    {
        PUTBUFFER
        PUTWRITEIDX
        GETREADIDX
    }

    GROUP : > CPU2TOCPU1RAM, PAGE = 1
    {
        GETBUFFER :    TYPE = DSECT
        GETWRITEIDX :  TYPE = DSECT
        PUTREADIDX :   TYPE = DSECT
    }
}

/*
//===========================================================================
// End of file.
//===========================================================================
*/
/*
 * Can_Regs.hpp
 *
 *  Created on: Mar 19, 2020
 *      Author: chaparrojd
 */

#ifndef INCLUDE_F2837XD_CAN_IMPLEMENTATION_CAN_REGS_HPP_
#define INCLUDE_F2837XD_CAN_IMPLEMENTATION_CAN_REGS_HPP_


#include <Interface/Platform_Defines.hpp>
//#include <Source/Common/Regs/F2837xd_Can_Regs.hpp>


namespace f2837xd
{
    namespace can
    {
        namespace impl
        {

            namespace regs
            {
                extern "C"
                {

                    struct CAN_CTL_BITS
                    {
                        bp_16 Init:1;                      ///> 0 Initialization
                        bp_16 IE0:1;                       ///> 1 Interrupt line 0 Enable
                        bp_16 SIE:1;                       ///> 2 Status Change Interrupt Enable
                        bp_16 EIE:1;                       ///> 3 Error Interrupt Enable
                        bp_16 rsvd1:1;                     ///> 4 Reserved
                        bp_16 DAR:1;                       ///> 5 Disable Automatic Retransmission
                        bp_16 CCE:1;                       ///> 6 Configuration Change Enable
                        bp_16 Test:1;                      ///> 7 Test Mode Enable
                        bp_16 IDS:1;                       ///> 8 Interruption Debug Support Enable
                        bp_16 ABO:1;                       ///> 9 Auto-Bus-On Enable
                        bp_16 PMD:4;                       ///> 13:10 Parity on/off
                        bp_16 rsvd2:1;                     ///> 14 Reserved
                        bp_16 SWR:1;                       ///> 15 SW Reset Enable
                        bp_32 INITDBG:1;                   ///> 16 Debug Mode Status
                        bp_32 IE1:1;                       ///> 17 Interrupt line 1 Enable Disabled
                        bp_32 rsvd3:1;                     ///> 18 Reserved
                        bp_32 rsvd4:1;                     ///> 19 Reserved
                        bp_32 rsvd5:1;                     ///> 20 Reserved
                        bp_32 rsvd6:3;                     ///> 23:21 Reserved
                        bp_32 rsvd7:1;                     ///> 24 Reserved
                        bp_32 rsvd8:1;                     ///> 25 Reserved
                        bp_32 rsvd9:6;                     ///> 31:26 Reserved
                    };

                    union CAN_CTL_REG
                    {
                        bp_32  all;
                        struct  CAN_CTL_BITS  bit;
                    };

                    struct CAN_ES_BITS
                    {
                        bp_16 LEC:3;                       ///> 2:0 Last Error Code
                        bp_16 TxOk:1;                      ///> 3 Transmission status
                        bp_16 RxOk:1;                      ///> 4 Reception status
                        bp_16 EPass:1;                     ///> 5 Error Passive State
                        bp_16 EWarn:1;                     ///> 6 Warning State
                        bp_16 BOff:1;                      ///> 7 Bus-Off State
                        bp_16 PER:1;                       ///> 8 Parity Error Detected
                        bp_16 rsvd1:1;                     ///> 9 Reserved
                        bp_16 rsvd2:1;                     ///> 10 Reserved
                        bp_16 rsvd3:5;                     ///> 15:11 Reserved
                        bp_32 rsvd4:16;                    ///> 31:16 Reserved
                    };

                    union CAN_ES_REG
                    {
                        bp_32  all;
                        struct  CAN_ES_BITS  bit;
                    };

                    struct CAN_ERRC_BITS
                    {
                        bp_16 TEC:8;                       ///> 7:0 Transmit Error Counter
                        bp_16 REC:7;                       ///> 14:8 Receive Error Counter
                        bp_16 RP:1;                        ///> 15 Receive Error Passive
                        bp_32 rsvd1:16;                    ///> 31:16 Reserved
                    };

                    union CAN_ERRC_REG
                    {
                        bp_32  all;
                        struct  CAN_ERRC_BITS  bit;
                    };

                    struct CAN_BTR_BITS
                    {
                        bp_16 BRP:6;                       ///> 5:0 Baud Rate Prescaler
                        bp_16 SJW:2;                       ///> 7:6 Synchronization Jump Width
                        bp_16 TSEG1:4;                     ///> 11:8 Time segment
                        bp_16 TSEG2:3;                     ///> 14:12 Time segment
                        bp_16 rsvd1:1;                     ///> 15 Reserved
                        bp_32 BRPE:4;                      ///> 19:16 Baud Rate Prescaler Extension
                        bp_32 rsvd2:12;                    ///> 31:20 Reserved
                    };

                    union CAN_BTR_REG
                    {
                        bp_32  all;
                        struct  CAN_BTR_BITS  bit;
                    };

                    struct CAN_INT_BITS
                    {
                        bp_16 INT0ID:16;                   ///> 15:0 Interrupt Identifier
                        bp_32 INT1ID:8;                    ///> 23:16 Interrupt 1 Identifier
                        bp_32 rsvd1:8;                     ///> 31:24 Reserved
                    };

                    union CAN_INT_REG
                    {
                        bp_32  all;
                        struct  CAN_INT_BITS  bit;
                    };

                    struct CAN_TEST_BITS
                    {
                        bp_16 rsvd1:3;                     ///> 2:0 Reserved
                        bp_16 SILENT:1;                    ///> 3 Silent Mode
                        bp_16 LBACK:1;                     ///> 4 Loopback Mode
                        bp_16 TX:2;                        ///> 6:5 CANTX Pin Control
                        bp_16 RX:1;                        ///> 7 CANRX Pin Status
                        bp_16 EXL:1;                       ///> 8 External Loopback Mode
                        bp_16 RDA:1;                       ///> 9 RAM Direct Access Enable:
                        bp_16 rsvd2:6;                     ///> 15:10 Reserved
                        bp_32 rsvd3:16;                    ///> 31:16 Reserved
                    };

                    union CAN_TEST_REG
                    {
                        bp_32  all;
                        struct  CAN_TEST_BITS  bit;
                    };

                    struct CAN_PERR_BITS
                    {
                        bp_16 MSG_NUM:8;                   ///> 7:0 Message Number
                        bp_16 WORD_NUM:3;                  ///> 10:8 Word Number
                        bp_16 rsvd1:5;                     ///> 15:11 Reserved
                        bp_32 rsvd2:16;                    ///> 31:16 Reserved
                    };

                    union CAN_PERR_REG
                    {
                        bp_32  all;
                        struct  CAN_PERR_BITS  bit;
                    };

                    struct CAN_RAM_INIT_BITS
                    {
                        bp_16 KEY0:1;                      ///> 0 KEY0
                        bp_16 KEY1:1;                      ///> 1 KEY1
                        bp_16 KEY2:1;                      ///> 2 KEY2
                        bp_16 KEY3:1;                      ///> 3 KEY3
                        bp_16 CAN_RAM_INIT:1;              ///> 4 Initialize CAN Mailbox RAM
                        bp_16 RAM_INIT_DONE:1;             ///> 5 CAN RAM initialization complete
                        bp_16 rsvd1:10;                    ///> 15:6 Reserved
                        bp_32 rsvd2:16;                    ///> 31:16 Reserved
                    };

                    union CAN_RAM_INIT_REG
                    {
                        bp_32  all;
                        struct  CAN_RAM_INIT_BITS  bit;
                    };

                    struct CAN_GLB_INT_EN_BITS
                    {
                        bp_16 GLBINT0_EN:1;                ///> 0 Global Interrupt Enable for  CAN INT0
                        bp_16 GLBINT1_EN:1;                ///> 1 Global Interrupt Enable for  CAN INT1
                        bp_16 rsvd1:14;                    ///> 15:2 Reserved
                        bp_32 rsvd2:16;                    ///> 31:16 Reserved
                    };

                    union CAN_GLB_INT_EN_REG
                    {
                        bp_32  all;
                        struct  CAN_GLB_INT_EN_BITS  bit;
                    };

                    struct CAN_GLB_INT_FLG_BITS
                    {
                        bp_16 INT0_FLG:1;                  ///> 0 Global Interrupt Flag for CAN INT0
                        bp_16 INT1_FLG:1;                  ///> 1 Global Interrupt Flag for CAN INT1
                        bp_16 rsvd1:14;                    ///> 15:2 Reserved
                        bp_32 rsvd2:16;                    ///> 31:16 Reserved
                    };

                    union CAN_GLB_INT_FLG_REG
                    {
                        bp_32  all;
                        struct  CAN_GLB_INT_FLG_BITS  bit;
                    };

                    struct CAN_GLB_INT_CLR_BITS
                    {
                        bp_16 INT0_FLG_CLR:1;              ///> 0 Global Interrupt flag clear for CAN INT0
                        bp_16 INT1_FLG_CLR:1;              ///> 1 Global Interrupt flag  clear for CAN INT1
                        bp_16 rsvd1:14;                    ///> 15:2 Reserved
                        bp_32 rsvd2:16;                    ///> 31:16 Reserved
                    };

                    union CAN_GLB_INT_CLR_REG
                    {
                        bp_32  all;
                        struct  CAN_GLB_INT_CLR_BITS  bit;
                    };

                    struct CAN_ABOTR_BITS
                    {
                        bp_32 abotr:32;
                    };

                    union CAN_ABOTR_REG
                    {
                        bp_32  all;
                        struct  CAN_ABOTR_BITS  bit;
                    };

                    struct CAN_TXRQ_X_BITS
                    {
                        bp_16 TxRqstReg1:2;                ///> 1:0 Transmit Request Register 1
                        bp_16 TxRqstReg2:2;                ///> 3:2 Transmit Request Register 2
                        bp_16 rsvd1:12;                    ///> 15:4 Reserved
                        bp_32 rsvd2:16;                    ///> 31:16 Reserved
                    };

                    union CAN_TXRQ_X_REG
                    {
                        bp_32  all;
                        struct  CAN_TXRQ_X_BITS  bit;
                    };

                    struct CAN_TXRQ_21_BITS
                    {
                        bp_32 TxRqst:32;                    ///> 31:16 Reserved
                    };

                    union CAN_TXRQ_21_REG
                    {
                        bp_32  all;
                        struct  CAN_TXRQ_21_BITS  bit;
                    };

                    struct CAN_NDAT_X_BITS
                    {
                        bp_16 NewDatReg1:2;                ///> 1:0 New Data Register 1
                        bp_16 NewDatReg2:2;                ///> 3:2 New Data Register 2
                        bp_16 rsvd1:12;                    ///> 15:4 Reserved
                        bp_32 rsvd2:16;                    ///> 31:16 Reserved
                    };

                    union CAN_NDAT_X_REG
                    {
                        bp_32  all;
                        struct  CAN_NDAT_X_BITS  bit;
                    };

                    struct CAN_NDAT_21_BITS
                    {
                        bp_32 NewDat:32;                ///> 1:0 New Data Register 1
                    };

                    union CAN_NDAT_21_REG
                    {
                        bp_32  all;
                        struct  CAN_NDAT_21_BITS  bit;
                    };

                    struct CAN_IPEN_X_BITS
                    {
                        bp_16 IntPndReg1:2;                ///> 1:0 Interrupt Pending Register 1
                        bp_16 IntPndReg2:2;                ///> 3:2 Interrupt Pending Register 2
                        bp_16 rsvd1:12;                    ///> 15:4 Reserved
                        bp_32 rsvd2:16;                    ///> 31:16 Reserved
                    };

                    union CAN_IPEN_X_REG
                    {
                        bp_32  all;
                        struct  CAN_IPEN_X_BITS  bit;
                    };

                    struct CAN_IPEN_21_BITS
                    {
                        bp_32 IntPnd:32;                ///> 1:0 Interrupt Pending Register 1
                    };

                    union CAN_IPEN_21_REG
                    {
                        bp_32  all;
                        struct  CAN_IPEN_21_BITS  bit;
                    };

                    struct CAN_MVAL_X_BITS
                    {
                        bp_16 MsgValReg1:2;                ///> 1:0 Message Valid Register 1
                        bp_16 MsgValReg2:2;                ///> 3:2 Message Valid Register 2
                        bp_16 rsvd1:12;                    ///> 15:4 Reserved
                        bp_32 rsvd2:16;                    ///> 31:16 Reserved
                    };

                    union CAN_MVAL_X_REG
                    {
                        bp_32  all;
                        struct  CAN_MVAL_X_BITS  bit;
                    };

                    struct CAN_MVAL_21_BITS
                    {
                        bp_32 MsgVal:32;                ///> 1:0 Message Valid Register 1
                    };

                    union CAN_MVAL_21_REG
                    {
                        bp_32  all;
                        struct  CAN_MVAL_21_BITS  bit;
                    };

                    struct CAN_IP_MUX21_BITS
                    {
                        bp_32 IntMux:32;                ///> 1:0 Message Valid Register 1
                    };

                    union CAN_IP_MUX21_REG
                    {
                        bp_32  all;
                        struct  CAN_IP_MUX21_BITS  bit;
                    };


                    struct CAN_IF3UPD_BITS
                    {
                        bp_32 IF3UpdEn:32;                ///> 1:0 Message Valid Register 1
                    };

                    union CAN_IF3UPD_REG
                    {
                        bp_32  all;
                        struct  CAN_IF3UPD_BITS  bit;
                    };

                    struct CAN_IFxCMD_BITS
                    {
                        bp_16 MSG_NUM:8;                   ///> 7:0 Message Number
                        bp_16 rsvd1:6;                     ///> 13:8 Reserved
                        bp_16 rsvd2:1;                     ///> 14 Reserved
                        bp_16 Busy:1;                      ///> 15 Busy Flag
                        bp_32 DATA_B:1;                    ///> 16 Access Data Bytes 4-7
                        bp_32 DATA_A:1;                    ///> 17 Access Data Bytes 0-3
                        bp_32 TXRQST:1;                    ///> 18 Access Transmission Request Bit
                        bp_32 ClrIntPnd:1;                 ///> 19 Clear Interrupt Pending Bit
                        bp_32 Control:1;                   ///> 20 Access Control Bits
                        bp_32 Arb:1;                       ///> 21 Access Arbitration Bits
                        bp_32 Mask:1;                      ///> 22 Access Mask Bits
                        bp_32 DIR:1;                       ///> 23 Write/Read Direction
                        bp_32 rsvd3:8;                     ///> 31:24 Reserved
                    };

                    union CAN_IFxCMD_REG
                    {
                        bp_32  all;
                        struct  CAN_IFxCMD_BITS  bit;
                    };

                    struct CAN_IFxMSK_BITS
                    {
                        bp_32 Msk:29;                      ///> 28:0 Identifier Mask
                        bp_32 rsvd1:1;                     ///> 29 Reserved
                        bp_32 MDir:1;                      ///> 30 Mask Message Direction
                        bp_32 MXtd:1;                      ///> 31 Mask Extended Identifier
                    };

                    union CAN_IFxMSK_REG
                    {
                        bp_32  all;
                        struct  CAN_IFxMSK_BITS  bit;
                    };

                    struct CAN_IFxARB_BITS
                    {
                        bp_32 ID:29;                       ///> 28:0 `
                        bp_32 Dir:1;                       ///> 29 Message Direction
                        bp_32 Xtd:1;                       ///> 30 Extended Identifier
                        bp_32 MsgVal:1;                    ///> 31 Message Valid
                    };

                    union CAN_IFxARB_REG
                    {
                        bp_32  all;
                        struct  CAN_IFxARB_BITS  bit;
                    };

                    struct CAN_IFxMCTL_BITS
                    {
                        bp_16 DLC:4;                       ///> 3:0 Data length code
                        bp_16 rsvd1:3;                     ///> 6:4 Reserved
                        bp_16 EoB:1;                       ///> 7 End of Block
                        bp_16 TxRqst:1;                    ///> 8 Transmit Request
                        bp_16 RmtEn:1;                     ///> 9 Remote Enable
                        bp_16 RxIE:1;                      ///> 10 Receive Interrupt Enable
                        bp_16 TxIE:1;                      ///> 11 Transmit Interrupt Enable
                        bp_16 UMask:1;                     ///> 12 Use Acceptance Mask
                        bp_16 IntPnd:1;                    ///> 13 Interrupt Pending
                        bp_16 MsgLst:1;                    ///> 14 Message Lost
                        bp_16 NewDat:1;                    ///> 15 New Data
                        bp_32 rsvd2:16;                    ///> 31:16 Reserved
                    };

                    union CAN_IFxMCTL_REG
                    {
                        bp_32  all;
                        struct  CAN_IFxMCTL_BITS  bit;
                    };

                    struct CAN_IFxDATA_BITS
                    {
                        bp_16 Data_0:8;                    ///> 7:0 Data Byte 0
                        bp_16 Data_1:8;                    ///> 15:8 Data Byte 1
                        bp_32 Data_2:8;                    ///> 23:16 Data Byte 2
                        bp_32 Data_3:8;                    ///> 31:24 Data Byte 3
                    };

                    union CAN_IFxDATA_REG
                    {
                        bp_32  all;
                        struct  CAN_IFxDATA_BITS  bit;
                    };

                    struct CAN_IFxDATB_BITS
                    {
                        bp_16 Data_4:8;                    ///> 7:0 Data Byte 4
                        bp_16 Data_5:8;                    ///> 15:8 Data Byte 5
                        bp_32 Data_6:8;                    ///> 23:16 Data Byte 6
                        bp_32 Data_7:8;                    ///> 31:24 Data Byte 7
                    };

                    union CAN_IFxDATB_REG
                    {
                        bp_32  all;
                        struct  CAN_IFxDATB_BITS  bit;
                    };

                    struct CAN_IF3OBS_BITS
                    {
                        bp_16 Mask:1;                      ///> 0 Mask data read observation
                        bp_16 Arb:1;                       ///> 1 Arbitration data read observation
                        bp_16 Ctrl:1;                      ///> 2 Ctrl read observation
                        bp_16 Data_A:1;                    ///> 3 Data A read observation
                        bp_16 Data_B:1;                    ///> 4 Data B read observation
                        bp_16 rsvd1:3;                     ///> 7:5 Reserved
                        bp_16 IF3SM:1;                     ///> 8 IF3 Status of Mask data read access
                        bp_16 IF3SA:1;                     ///> 9 IF3 Status of Arbitration data read access
                        bp_16 IF3SC:1;                     ///> 10 IF3 Status of Control bits read access
                        bp_16 IF3SDA:1;                    ///> 11 IF3 Status of Data A read access
                        bp_16 IF3SDB:1;                    ///> 12 IF3 Status of Data B read access
                        bp_16 rsvd2:2;                     ///> 14:13 Reserved
                        bp_16 IF3Upd:1;                    ///> 15 IF3 Update Data
                        bp_32 rsvd3:16;                    ///> 31:16 Reserved
                    };

                    union CAN_IF3OBS_REG
                    {
                        bp_32  all;
                        struct  CAN_IF3OBS_BITS  bit;
                    };

                    struct CAN_IF3MSK_BITS
                    {
                        bp_32 Msk:29;                      ///> 28:0 Mask
                        bp_32 rsvd1:1;                     ///> 29 Reserved
                        bp_32 MDir:1;                      ///> 30 Mask Message Direction
                        bp_32 MXtd:1;                      ///> 31 Mask Extended Identifier
                    };

                    union CAN_IF3MSK_REG
                    {
                        bp_32  all;
                        struct  CAN_IF3MSK_BITS  bit;
                    };

                    struct CAN_IF3ARB_BITS
                    {
                        bp_32 ID:29;                       ///> 28:0 Message  Identifier
                        bp_32 Dir:1;                       ///> 29 Message Direction
                        bp_32 Xtd:1;                       ///> 30 Extended Identifier
                        bp_32 MsgVal:1;                    ///> 31 Message Valid
                    };

                    union CAN_IF3ARB_REG
                    {
                        bp_32  all;
                        struct  CAN_IF3ARB_BITS  bit;
                    };

                    struct CAN_IF3MCTL_BITS
                    {
                        bp_16 DLC:4;                       ///> 3:0 Data length code
                        bp_16 rsvd1:3;                     ///> 6:4 Reserved
                        bp_16 EoB:1;                       ///> 7 End of Block
                        bp_16 TxRqst:1;                    ///> 8 Transmit Request
                        bp_16 RmtEn:1;                     ///> 9 Remote Enable
                        bp_16 RxIE:1;                      ///> 10 Receive Interrupt Enable
                        bp_16 TxIE:1;                      ///> 11 Transmit Interrupt Enable
                        bp_16 UMask:1;                     ///> 12 Use Acceptance Mask
                        bp_16 IntPnd:1;                    ///> 13 Interrupt Pending
                        bp_16 MsgLst:1;                    ///> 14 Message Lost
                        bp_16 NewDat:1;                    ///> 15 New Data
                        bp_32 rsvd2:16;                    ///> 31:16 Reserved
                    };

                    union CAN_IF3MCTL_REG
                    {
                        bp_32  all;
                        struct  CAN_IF3MCTL_BITS  bit;
                    };

                    struct CAN_IF3DATA_BITS
                    {
                        bp_16 Data_0:8;                    ///> 7:0 Data Byte 0
                        bp_16 Data_1:8;                    ///> 15:8 Data Byte 1
                        bp_32 Data_2:8;                    ///> 23:16 Data Byte 2
                        bp_32 Data_3:8;                    ///> 31:24 Data Byte 3
                    };

                    union CAN_IF3DATA_REG
                    {
                        bp_32  all;
                        struct  CAN_IF3DATA_BITS  bit;
                    };

                    struct CAN_IF3DATB_BITS
                    {
                        bp_16 Data_4:8;                    ///> 7:0 Data Byte 4
                        bp_16 Data_5:8;                    ///> 15:8 Data Byte 5
                        bp_32 Data_6:8;                    ///> 23:16 Data Byte 6
                        bp_32 Data_7:8;                    ///> 31:24 Data Byte 7
                    };

                    union CAN_IF3DATB_REG
                    {
                        bp_32  all;
                        struct  CAN_IF3DATB_BITS  bit;
                    };

                    struct CAN_REGS
                    {
                        union   CAN_CTL_REG                      CAN_CTL;                      ///> CAN Control Register
                        union   CAN_ES_REG                       CAN_ES;                       ///> Error and Status Register
                        union   CAN_ERRC_REG                     CAN_ERRC;                     ///> Error Counter Register
                        union   CAN_BTR_REG                      CAN_BTR;                      ///> Bit Timing Register
                        union   CAN_INT_REG                      CAN_INT;                      ///> Interrupt Register
                        union   CAN_TEST_REG                     CAN_TEST;                     ///> Test Register
                        uint32_t                                 rsvd1[2];                     ///> Reserved
                        union   CAN_PERR_REG                     CAN_PERR;                     ///> CAN Parity Error Code Register
                        uint32_t                                 rsvd2[16];                    ///> Reserved
                        union   CAN_RAM_INIT_REG                 CAN_RAM_INIT;                 ///> CAN RAM Initialization Register
                        uint32_t                                 rsvd3[6];                     ///> Reserved
                        union   CAN_GLB_INT_EN_REG               CAN_GLB_INT_EN;               ///> CAN Global Interrupt Enable Register
                        union   CAN_GLB_INT_FLG_REG              CAN_GLB_INT_FLG;              ///> CAN Global Interrupt Flag Register
                        union   CAN_GLB_INT_CLR_REG              CAN_GLB_INT_CLR;              ///> CAN Global Interrupt Clear Register
                        uint32_t                                 rsvd4[18];                    ///> Reserved
                        union CAN_ABOTR_REG                      CAN_ABOTR;                    ///> Auto-Bus-On Time Register
                        union   CAN_TXRQ_X_REG                   CAN_TXRQ_X;                   ///> CAN Transmission Request Register
                        union   CAN_TXRQ_21_REG                  CAN_TXRQ_21;                  ///> CAN Transmission Request 2_1 Register
                        uint32_t                                 rsvd5[6];                     ///> Reserved
                        union   CAN_NDAT_X_REG                   CAN_NDAT_X;                   ///> CAN New Data Register
                        union   CAN_NDAT_21_REG                  CAN_NDAT_21;                  ///> CAN New Data 2_1 Register
                        uint32_t                                 rsvd6[6];                     ///> Reserved
                        union   CAN_IPEN_X_REG                   CAN_IPEN_X;                   ///> CAN Interrupt Pending Register
                        union   CAN_IPEN_21_REG                  CAN_IPEN_21;                  ///> CAN Interrupt Pending 2_1 Register
                        uint32_t                                 rsvd7[6];                     ///> Reserved
                        union   CAN_MVAL_X_REG                   CAN_MVAL_X;                   ///> CAN Message Valid Register
                        union   CAN_MVAL_21_REG                  CAN_MVAL_21;                  ///> CAN Message Valid 2_1 Register
                        uint32_t                                 rsvd8[8];                     ///> Reserved
                        union   CAN_IP_MUX21_REG                 CAN_IP_MUX21;                 ///> CAN Interrupt Multiplexer 2_1 Register
                        uint32_t                                 rsvd9[18];                    ///> Reserved
                        union   CAN_IFxCMD_REG                   CAN_IF1CMD;                   ///> IF1 Command Register
                        union   CAN_IFxMSK_REG                   CAN_IF1MSK;                   ///> IF1 Mask Register
                        union   CAN_IFxARB_REG                   CAN_IF1ARB;                   ///> IF1 Arbitration Register
                        union   CAN_IFxMCTL_REG                  CAN_IF1MCTL;                  ///> IF1 Message Control Register
                        union   CAN_IFxDATA_REG                  CAN_IF1DATA;                  ///> IF1 Data A Register
                        union   CAN_IFxDATB_REG                  CAN_IF1DATB;                  ///> IF1 Data B Register
                        uint32_t                                 rsvd10[4];                    ///> Reserved
                        union   CAN_IFxCMD_REG                   CAN_IF2CMD;                   ///> IF2 Command Register
                        union   CAN_IFxMSK_REG                   CAN_IF2MSK;                   ///> IF2 Mask Register
                        union   CAN_IFxARB_REG                   CAN_IF2ARB;                   ///> IF2 Arbitration Register
                        union   CAN_IFxMCTL_REG                  CAN_IF2MCTL;                  ///> IF2 Message Control Register
                        union   CAN_IFxDATA_REG                  CAN_IF2DATA;                  ///> IF2 Data A Register
                        union   CAN_IFxDATB_REG                  CAN_IF2DATB;                  ///> IF2 Data B Register
                        uint32_t                                 rsvd11[4];                    ///> Reserved
                        union   CAN_IF3OBS_REG                   CAN_IF3OBS;                   ///> IF3 Observation Register
                        union   CAN_IF3MSK_REG                   CAN_IF3MSK;                   ///> IF3 Mask Register
                        union   CAN_IF3ARB_REG                   CAN_IF3ARB;                   ///> IF3 Arbitration Register
                        union   CAN_IF3MCTL_REG                  CAN_IF3MCTL;                  ///> IF3 Message Control Register
                        union   CAN_IF3DATA_REG                  CAN_IF3DATA;                  ///> IF3 Data A Register
                        union   CAN_IF3DATB_REG                  CAN_IF3DATB;                  ///> IF3 Data B Register
                        uint32_t                                 rsvd12[4];                    ///> Reserved
                        union   CAN_IF3UPD_REG                   CAN_IF3UPD;                   ///> IF3 Update Enable Register
                    };
                }
            }

        }
    }
}


#endif /* INCLUDE_F2837XD_CAN_IMPLEMENTATION_CAN_REGS_HPP_ */