Tool/software: Code Composer Studio
I'm following up on this exact issue.
I've narrowed down the issue to the a C/IO 'Process CIO'. Error 0x90000008/-1060
trgmsg.obj (:text:_writemsg) from rts67plus.lib.
Regards,
Blake West
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Code Composer Studio
I'm following up on this exact issue.
I've narrowed down the issue to the a C/IO 'Process CIO'. Error 0x90000008/-1060
trgmsg.obj (:text:_writemsg) from rts67plus.lib.
Regards,
Blake West
Hi Ki,
This building on the previous issue. I'm a team member taking over this issue.
Currently I'm running what was mentioned previously. XDS510 Debugger.
This issue occurs when I try to do a GEL_reset() via GEL scripting. It comes out with this error: 0x80000008 / -1060 from a rts67plus.lib Process CIO.
I've been able to resolve this by adding resetGelState() before the GEL_reset() in a gel MenuFunction
Regards,
Blake
Got it. Thanks for the extra information and also for sharing your workaround.
ki
Blake, just to set expectations correctly - CCSv3.3 is not supported anymore. If there are any bugs identified with CCSv3.3, there are no plans to fix them. Most we can do is a cursory investigation and see if there are any (other) workarounds.
ki