This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Compiler/CCSTUDIO-C2000: Need code gen tools prior to version 4.1.0.

Part Number: CCSTUDIO-C2000

Tool/software: TI C/C++ Compiler

George Mock previously sent me the 4.1.0 C2000 compiler but we determined that version is not exactly what we need. We are attempting to compile existing C code and match a binary that we have. We have determined that the code generation is VERY close to matching but is not there yet. We have previously tried the 5.2.1 and 5.1.6 compilers which generate code that deviates from our binary much more than the 4.1.0 version which indicates we need to continue to move backwards in version.

There is also a specific signature in the RTS library that is different in the binary than what is provided in the 5.2.1, 5.1.6 and 4.1.0 compilers.

Is there any chance we could get access to a version of the C2000 compiler somewhat earlier than 4.1.0 and I can check the RTS signature. Sorry to bother you with a request for a non-specific compiler version number.

Thanks,

Drake