This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/CC3220SF-LAUNCHXL: XGCONF editor on CCS version 10

Part Number: CC3220SF-LAUNCHXL
Other Parts Discussed in Thread: CC3220SF

Tool/software: Code Composer Studio

Hi

I can not find editor XGCONF on CCS version 10

  • Hello,

    Fernando Dias2 said:
    I can not find editor XGCONF on CCS version 10

    right-click on the cfg file you wish to open in XGCONF and select:

    Once this is done once, CCS should remember the next time you wish to open the file.

    Thanks

    ki

  • Hi Ki

    Thanks for your reply and it is  correct, but seems I can not find the file with extension CFG, do I need to create it , when import from Demos TIRTOS or Examples TIRTOS ?

    I have imported a ccs project to my CCS ( working with launchpad CC3220SF ) named as  provisioning_CC3220SF_LAUNCHXL_tirtos_ccs,

    I can not see any file with extension *.cfg on the project tree.

    Just inform is active as ( Active-Debug ).

    I have tried import another project TIRTOS , such as network terminal , and still can not find the *.cfg file.

    Thanks in advance

  • TI-RTOS projects will have a BIOS configuration file (*.cfg). When you imported the provisioning_CC3220SF_LAUNCHXL_tirtos_ccs project, a dependent tirtos_builds_CC3220SF_LAUNCHXL_release_ccs project should have also been imported with it. That project is the dependent TI-RTOS project that provisioning_CC3220SF_LAUNCHXL_tirtos_ccs is dependent on. It had a cfg file (release.cfg) that you can open with XGCONF. Many of the SimpleLink examples take this approach where they have all the kernel content in a separate TI-RTOS project.

    Thanks

    ki