Part Number: IWR1843BOOST
Other Parts Discussed in Thread: IWR1843, UNIFLASH
Tool/software: Code Composer Studio
hello:
We are getting following error when we debug iwr1843boost and unable to proceed forward.
Development platform information is as follows:
Hardware platform: IWR1843BOOST
SDK version: mmwave_sdk_03_03_00_03
CCS version: Code Composer Studio 9.2.0
The debug step:
1:open CCS9.2 Resource Explorer->softsore->sensor->industrial_toolbox_4_2_1->labs->traffic_monitoring import 18xx-DSS and 18xx MSS projects
2:compile 18xx-DSS and 18xx MSS projects get traffic_monitoring_18xx_mss.xer4f and traffic_monitoring_18xx_dss.xe674
3:Download the xwr18xx_radarss_rprc.bin file before debugging with unflash5.1.0
4:through IWR1843.ccxml file debug
debug errors:
The following error occurred when the MSS program was running at this location:
The main errors are as follows:
Exception occurred in ThreadType_Task.
Task handle: 0x8006d60.
Task stack base: 0x20202020.
Task stack size: 0x20202020.
R0 = 0x20202020 R8 = 0x20202020
R1 = 0x20202020 R9 = 0x08001d68
R2 = 0x00025a74 R10 = 0x00000000
R3 = 0x00000010 R11 = 0x0801b9a4
R4 = 0x0801b9a4 R12 = 0x00025a74
R5 = 0x00000007 SP(R13) = 0x08006dd8
R6 = 0x08006d60 LR(R14) = 0x00007bcf
R7 = 0x20202020 PC(R15) = 0x00019f00
PSR = 0x800c019f
DFSR = 0x0000080d IFSR = 0x00000000
DFAR = 0x20202020 IFAR = 0x00000000
{module#43}: line 205: error {id:0x1a0000, args:[0x19f00, 0x7bcf]}
xdc.runtime.Error.raise: terminating execution
error 2:
This window appears whenever I download the program
Please help me
Thank you very much