This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Code Composer Studio
Hello,
CCS Version: 9.2.0.00013
CC1352 SDK: simplelink_cc13x2_26x2_sdk_3_30_00_03
I am working on sensor example. I created workspace ,imported sensor example and build that project. When I reopen workspace, getting "Cannot determine URI for '/sensor_CC1352R1_LAUNCHXL_tirtos_ccs_syscfg/application/main.c' " problem. why am i getting this problem and how can I overcome this problem??
Hello Ki,
First I exported project from previous workspace in zip format.
I imported this zip file in my new workspace.
When I reopen workspace for first 3 to 4 times not getting problem. But after sometimes getting cannot determin URI problem.
Is the issue that you are not allowed to share your project, or that the forum itself is not allowing you to upload the zip?
Can you at least share just the project metadata files (the three .*project files in the project folder)?
Thanks
ki