This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/LAUNCHXL2-RM57L: GRAPHS DON'T SHOW UP

Part Number: LAUNCHXL2-RM57L

Tool/software: Code Composer Studio

Hello 

Currently, I'm working with the Hercules RM57 Launchpad

During debugging, I'm tried to show the graphs of an array, however, when I click in graph option in expressions window, CCS only opens a blank window without a name, as we see below.

I found the same problem in CCSv9, then, I installed CCSv10, also, I tried with the delete of cache files as recommend in other e2e forums, however, the problem persists. 

Carlos. R