Part Number: TMS320F28075
Other Parts Discussed in Thread: C2000WARE
Tool/software: Code Composer Studio
Hi,
I'm using CCS8.3.1, and I import the example project from the file below: (without click "copy project into workspace")
C:\ti\c2000\C2000Ware_1_00_06_00\device_support\f2807x\examples\cpu1\can_loopback\cpu01
There is no cmd file in the directory.
Then I wonder how does the project knows which cmd file to use?
If I copy a F28075.cmd file directly into the directory C:\ti\c2000\C2000Ware_1_00_06_00\device_support\f2807x\examples\cpu1\can_loopback\cpu01, will it use this cmd file automatically.
Thanks.