This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/CODECOMPOSER: Compilier makes error

Part Number: CODECOMPOSER

Tool/software: Code Composer Studio

This code never exits the loop. LongCount is incremented in an interrupt

void mSWait( unsigned int WaitDuration )  // measured in units of 1 ms
{
  unsigned int msTimer = LongCount;
    while((LongCount - msTimer) < WaitDuration);
}
This is the dissassembly
      mSWait():
b208:   421E 0488           MOV.W   &LongCount,R14
      $C$L2:b20c:   4E0F                MOV.W   R14,R15
b20e:   8E0F                SUB.W   R14,R15
b210:   9C0F                CMP.W   R12,R15
b212:   2BFC                JLO     ($C$L2)
b214:   4130                RET
no surprise that it never exits since &LongCount is not read inside the loop

Same with this code:
void mSWait( unsigned int WaitDuration )  // measured in units of 1 ms
{
  unsigned int msTimer = LongCount;
  unsigned int x;
  do  x=LongCount - msTimer - WaitDuration;
  while( x );
}   

however changing the while to while(x<0) works. The irony is that the compiler says that it is a pointless comparison. Help!