Part Number: TM4C1292NCPDT
Tool/software: Code Composer Studio
Hello,
I have been working with XDS100V2 debugger without any issues and all of a sudden started reporting connecting error due to the following reason. I am using code composer 9.3 (windows 10) and tried all forums for any direction and couldn't find anything that cleared my connecting issue. However I have no trouble connection and debugging with CCS 8.2 (so I am using 8.2 for now until I can get V9.3 going).
I tried uninstalling and reinstalling drivers, CCS9.3 (an even tried CCS v10) etc and still cannot connect. Any help is greatly appreciated.
Many thanks
Gamini
Error Message:
This utility has selected a 100- or 510-class product.
This utility will load the adapter 'jioserdesusb.dll'.
An error occurred while soft opening the controller.
-----[An error has occurred and this utility has aborted]--------------------
This error is generated by TI's USCIF driver or utilities.
The value is '-716' (0xfffffd34).
The title is 'SC_ERR_LIB_LOAD_SERDES_DRV'.
The explanation is:
Required dynamic library jscserdes could not be located.
The library isn't on the search path.