Other Parts Discussed in Thread: TMS320F28027
Tool/software: Code Composer Studio
hi to all,
I recently update CCS from 9.1 to 9.3 and im unable to debug program on tms320f28027 and the tms32028379D. Im using linux Tumbleweed as main OS. I can't detect the emulators.
checking the targetConfigs I got:
This error is generated by TI's USCIF driver or utilities. The value is '-151' (0xffffff69). The title is 'SC_ERR_FTDI_OPEN'. The explanation is: One of the FTDI driver functions used during the connect returned bad status or an error. The cause may be one or more of: no XDS100 is plugged in, invalid XDS100 serial number, blank XDS100 EEPROM, missing FTDI drivers, faulty USB cable. Use the xds100serial command-line utility in the 'common/uscif' folder to verify the XDS100 can be located. [End: Texas Instruments XDS100v1 USB Debug Probe_0]
by running the lsusb command in console i can't find the drivers for the ftdi. I install drivers from install_scripts folder in CCS and reboot many times without succed.
Gastón