Other Parts Discussed in Thread: MSP430F5418A, MSP430F5418
I have a customer (Ricoh) who is using the MSP430F5418A device which has 128KB od code memory. In production they plan to Use a Data I/O FlashPak III programmer at their facility in Asia. I have attached to this post a copy of the file formats supported by Data I/O. This raises some questions.
1 - Is the .out file from CCS4 COFF ?
2 - What is the format of the .obj file? it looks unique to TI.
3- Which Intel hex file format is used when Intel hex is choosen? It appears to be the original 8-bit Intel Hex format which has a limit of 64KB of code space.
Do you have any answer to address the needs of this customer? My customer would appreciate a quick response, if possible.
Thanks - Bill